Siemens has developed a comprehensive concept for energy systems worldwide – the first such concept that takes into account and brings together not only technology but also the areas of regulation and social engagement. The Energy Value Charter aims to create customized solutions that will empower countries to make their energy systems fit for the future. The concept encompasses suggestions for implementing sustainable power-generation technologies, together with recommendations on how legal frameworks must be adapted to ensure that the full potential of these technologies can be tapped. In addition, the concept specifies options for promoting social engagement, such as work-study programs, as well as for refinancing infrastructure while simultaneously reducing greenhouse gas emissions. Siemens presented the concept at the 2019 Energy Transition Dialogue in Berlin, in the presence of energy ministers from a range of countries.
Siemens developed the concept to create a global framework for energy solutions for its businesses. With its Energy Value Charter, the company wants to enter into a dialogue with governments in order to shape energy systems in such a way that they provide the basis for economic growth, social engagement and sustainable development.
On September 26, 2017 Siemens and Alstom have signed a Memorandum of Understanding to combine Siemens' mobility business, including its rail traction drives business, with Alstom. The transaction brings together two innovative players of the railway market with unique customer value and operational potential. The two businesses are largely complementary in terms of activities and geographies. Siemens will receive newly issued shares in the combined company representing 50 percent of Alstom's share capital on a fully diluted basis.On February 6, 2019 the European Commission has announced its decision to prohibit the proposed combination of the Siemens and Alstom mobility businesses. As a result of this prohibition, the merger will not proceed. Siemens and Alstom regret that the remedies they offered, including recent improvements, have been considered insufficient by the EU Commission.
The Siemens Zug campus features a new office building with 1,000 work spaces and a newly constructed production building. The Siemens Zug campus is one of the first new projects to use Building Information Modeling (BIM) for design and construction. The campus complex is equipped with building automation, security and fire safety technology from Siemens BT and particular emphasis was placed on sustainability and energy efficiency of the buildings.
The Fund for the Future that Siemens and the company’s Central Works Council agreed to establish in May 2018 is now available to finance qualification projects in Germany. Until the end of fiscal 2022, Siemens will provide up to €100 million for such projects, in addition to the company’s regular annual budget of around €500 million for training and continuing education, thereof €290 million in Germany. The Fund for the Future is a key element with which Siemens and the Central Works Council are shaping the structural transformation of today’s economy – a transformation that is changing the working world to an unimaginable degree. Siemens, the company's Central Works Council and the IG Metall labor union agreed on a Future Pact in May 2018. This pact, which includes the Fund for the Future, established the main framework for addressing the structural transformation now taking place in Germany.
Additive manufacturing has the potential to become a new key technology. For example it opens up new attractive prospects in the manufacture of gas turbines. This is why Siemens has been investing in this innovative technology right from its inception, and is now driving the industrialization and commercialization of these processes. Additive Manufacturing is a process that builds parts layer-by-layer from sliced CAD models to form solid objects. This enables highly precise solutions to be formed from powdered high-performance materials. Siemens is a pioneer in Additive Manufacturing and already uses the technology for rapid prototyping. Furthermore the company is now developing solutions ready for series-production for manufacturing gas turbine burner nozzles and repairing burner heads. Just recently Siemens achieved yet another breakthrough: the first gas turbine blades ever to be produced using Additive Manufacturing have successfully finished performance testing under full-load conditions.
On March 2nd, 2017, German Chancellor Angela Merkel, Egyptian President Abdel Fattah El-Sisi, Siemens CEO Joe Kaeser and further high-ranking representatives witnessed the symbolic inauguration of the first phase of Siemens' megaproject in Egypt. The event marked an important milestone towards the completion of the project.
In collaboration with the Egyptian Ministry of Electricity and Renewable Energy, Siemens and its consortium partners, Orascom Construction and Elsewedy Electric, announced on July 24, 2018 the completion of the Egypt Megaproject in record time. The parties celebrated the combined cycle commissioning and the start of operations at the Beni Suef, Burullus and New Capital power plants. The stations will add a total of 14.4 gigawatts (GW) of power generation capacity to Egypt's national grid, enough power to supply up to 40 million people with reliable electricity. With this milestone, Egypt and Siemens have set a new world record for execution of modern, fast-track power projects, delivering 14.4 GW of power in only 27.5 months. A single combined cycle power plant block with a capacity of 1,200 megawatts typically takes approximately 30 months for construction. For the Egypt Megaproject Siemens in parallel built twelve of these blocks in record time and connected them to the grid.
Following the delivery of several Siemens SGT5-8000H gas turbines, the first steam turbine for the Egypt Megaproject began its journey in December 2016 from the Siemens factory in Muelheim to the power plant Beni Suef in Egypt. The main components of the 670-ton cargo were lifted with a heavy-duty crane from the production hall onto a transport vessel standing by at the plant's inland harbor facilities. The vessel transported the SST-5000 steam turbine from Muelheim to the deep-water port of Antwerp where it was loaded onto a heavy cargo ship and transported to Egypt.
After the steam turbines installation, the waste heat from the gas turbines will be used to produce steam that will then drive the steam turbine, thus increasing the overall power output and efficiency of the power plant. In total, Siemens will deliver twelve SST-5000 steam turbines for the Egyptian power plants Beni Suef, Burullus and New Capital. All of these steam turbines will be manufactured at the Siemens factory in Muelheim.
At Siemens, Inclusion is a holistic mindset. Not only do we want to set an example of accessibility, we want to pave the way for inclusion in other companies. We have learned – you cannot prescribe inclusion in the interplay between man, environment and activity. You need to live accessibility and inclusion in the day to day. Our employees demonstrate how to overcome the “hurdles in the head” every single day – and we support them.
3i is the Siemens-wide program that promotes, implements and rewards employee ideas and initiatives. What is a good 3i idea? It is one that identifies "what" should be improved, outlines "how" something can be improved and explains "why" the idea's implementation will be a real improvement for our customers, employees and/or Siemens itself.
On January 24, 2018, the most powerful high-voltage direct-current (HVDC) transformer began its journey from the transformer factory in Nuremberg, Germany, to China. The transformer will first be transported to the harbor in Nuremberg by special heavy load transporter, where it will be loaded onto a ship. Its journey will take it to Rotterdam via the Main-Danube Canal, and from there it will be shipped to China, where it will arrive after several weeks on the high seas. In July 2016, Siemens received an order to manufacture four transformers of this type. About a year later, the world’s first 1,100 kV transformer was completed and successfully passed the tests in the testing facility. The enormous dimensions of the transformer – 37.5 meters long, 14.4 meters tall, and 12 meters wide – posed a logistical challenge for the team. In operation, the transformer weighs just under 900 tons and its efficiency is well above 99% of the rated power. For the first time, the transformer will enable a high-voltage direct-current (HVDC) transmission with low losses over a record distance of 3,284 kilometers with a transmission capacity of 12 gigawatts. HVDC transformers are part of the converter station that convert alternating current into direct current at the beginning of the transmission line and convert it back again at the end of the line. The conversion from alternating current to direct current helps to transmit energy over long distances with low losses. Transformers are key components of an HVDC line: Thanks to the transformer, the Changji-Guquan project will be able to transmit direct current with a huge 1,110 kilovolts for the first time in the world. The new transformer not only makes the transmission of this record voltage level possible, but it is also the world’s most powerful tested transformer with a capacity of 587 megavoltamperes. Siemens has thus achieved a new dimension in high-voltage direct-current transmission. The HVDC line between Changji and Guquan will be operated by State Grid Corporation (SGCC), a Chinese grid operator. The connection is expected to begin operation in 2019.