- Reliable protection with minimal space requirements
- For power distribution and industrial plants
Siemens Smart Infrastructure presents the new Siprotec 5 Compact device, specially designed to address the demands of industrial applications, infrastructure and distribution grids. With its compact size, large number of inputs and outputs, and universal range of functions, it can be configured to meet the specific requirements associated with protecting feeders and motors. As a space-saving universal device, it is ideally suited to help optimize investment and operating costs in power distribution.
- Improvement of machine tool availability through predictive maintenance with Analyze MyMachine /Condition
- Analyze MyMachine /Condition for Sinumerik Edge creates a mechanical fingerprint of the machine tool
- Condition evaluation, analysis and comparison of all connected machines using the Mindsphere application
Siemens is extending its edge application Analyze MyMachine /Condition with a corresponding Mindsphere application and thus demonstrating how edge computing and cloud computing can be intelligently combined. The Sinumerik Edge Application Analyze MyMachine /Condition, which the company presented last year at the EMO, uses high-frequency CNC data to create the mechanical fingerprint of a machine tool. In the application, users can capture and evaluate various parameters such as stiffness, friction, and backlash in the individual axes with the help of flexibly configurable measurement series. The measurement results can then be visualized and compared with reference data.
- Sinumerik One Dynamics - three technology packages to increase the efficiency of CNC users when programming in the shopfloor and executing CAM-generated CNC programs
- Top Surface and Top Speed Plus for excellent motion control and perfect workpiece surfaces
With the software version NCU-SW 6.14, Siemens is launching three powerful technology packages exclusively for the CNC Sinumerik One. The Sinumerik One Dynamics packages are available in three different packages: One Dynamics Operate, One Dynamics 3-axis milling and One Dynamics 5-axis milling. The software functions contained in the technology packages support users from machine-oriented programming in the jobshop to high-performance machining of CAD-CAM-programmed workpieces with high surface quality.
- Simotics S-1FS2 in stainless steel housing with specific features for use in the pharmaceutical and F&B industries
- Servo planetary gearmotors Simotics S-1FK2 for optimum adjustment of speed, torque and mass inertia
- Simotics S-1FT2 in protection class IP67 with 26 bit encoder, higher rated speed and other selectable features
Siemens is adding new servo motors to its proven Sinamics S210 single-cable servo drive system, thereby expanding its range of applications. Specifically, for use in the pharmaceutical and food industries, the company is launching the Simotics S-1FS2, a motor version with a stainless-steel housing, the highest degree of protection IP67/IP69, and high-resolution 22-bit absolute multiturn encoders. The servo motor thus meets all hygienic conditions and can be used for mixing and stirring, air conditioning and ventilating, dosing and filling, as well as conveying, packaging and storing a wide variety of end products in the food and beverage sector and in the pharmaceutical industry.
- New software for omnidirectional control
- 360-degree freedom of movement for AGVs
- Innovative steering system implemented with ebm-papst
Siemens has expanded Simove, the scalable automation solution for Automated Guided Vehicle (AGV)
applications, to include functionality for omnidirectional control. The new software supports unrestricted freedom of movement for AGVs. Together with Simatic
Micro-Drive, the new member of the Siemens converter family specifically for
the safety extra-low voltage range, plant and machine builders can create universal
and flexible systems. Together with partner ebm-papst an initial application example has been realized: a steering system that uses Simatic Micro-Drive,
the universal Simatic controller and the new control software from Simove. The
compact steering system features a special gearbox where the speeds of both
motors in the steering system are overlaid. This means that the steering system
does not require moving cables. The result is 360-degree rotational movement of
the wheel and therefore of the system. In addition, the high transmission in the
driving and steering direction provides a high level of control accuracy for
the system. Thanks to the integrated safety functions of the Simatic Micro-Drive,
safe control and monitoring of the integrated motors is ensured at all times.
- Eight desalination plants with process automation, drive technology, process instrumentation and communication technology
- Total capacity of 240,000 cubic meters per day
- Order volume is a double-digit million Euro figure
Siemens has received a follow-up order from the A3C consortium (Rawafid Industrial, Advanced Water Technology, SETE and Al Fatah) to equip eight seawater desalination plants in Saudi Arabia with electrical equipment. The new plants for seawater desalination using the principle of reverse osmosis are spread along the West coast of Saudi Arabia. The total capacity of the plants will be 240,000 cubic meters per day, with a power consumption of just three kilowatts per cubic meter of produced water, which is below the usual value and will provide significant energy savings. The scope of supply from Siemens includes hardware and software engineering, power distribution, PCS7 automation, medium and low voltage converters, Industrial Ethernet communication technology and process instrumentation for eight reverse osmosis plants, plus plant commissioning. The project will follow a tight schedule, with commissioning planned from autumn 2019.
- New “Location Intelligence” software expands Simatic RTLS locating platform to include digital twin of performance
- Visualized real-time analyses create potential for optimization and facilitate rapid decision-making
- Provides customers with overview of material flow and order information
Siemens introduces new “Location Intelligence” software, which expands the Simatic RTLS (Real-Time Locating System) locating platform to include the digital twin of performance. The web-based software analyzes and visualizes dynamic data, processes events, and can be addressed directly from local ERP (Enterprise Resource Planning) or MES (Manufacturing Execution System) systems. The intelligence acquired based on position data provides the user with a comprehensive overview of material flow, order information or possible problem areas.
- New Grid Diagnostic Suite offers unique comprehensive insights
- Gain a grid-wide view of energy automation systems
- Market launch of initially four cloud-enabled applications
- Enhances cost efficiency and availability of smart grids
- Support through digitalization in increasingly complex power grids
Siemens is presenting for the first time its new Grid Diagnostic Suite at the European Utility Week in Paris. The Grid Diagnostic Suite initially includes four cloud-based applications which collect data from new or existing field devices for protection, distribution automation and power quality. These data are stored and analyzed in the cloud. This requires almost no additional engineering effort. Distribution grid operators and operators of electricity grids in industrial parks can quickly tap into useful information from devices installed anywhere in the smart grid. This will enable grid faults, for example, to be detected at an early stage and quickly rectified. After information is collected, vulnerabilities can be identified, and necessary measures can be implemented before any damage occurs. In this way, Internet of Things (IoT) applications in the Grid Diagnostic Suite enhance the availability of power grids while enabling them to be operated cost-efficiently.
- Siemens presents liquid-cooled, robust power conversion system based on proven Sinamics S120 platform
- Grid converter comes with certification in accordance to VDE-AR-N 4110 and with validated simulation model for easy project planning, optimization and integration into the power grid
With Sinamics PCS, Siemens presents a new power conversion system for battery storage applications. The Sinamics PCS grid converter makes locally generated battery power usable for industrial and public power grids. Sinamics PCS controls the charging and discharging process of the battery and helps to handle load peaks and grid disturbances via the battery storage, to store the electricity in an energy- and cost-efficient manner and to bring the energy stored in batteries efficiently and reliably into the grid.
- System based on Siemens Spectrum Power supports second-by-second control of all assets and integration of RWE wind and solar farms
- Improved combination of electricity generation from renewables and conventional fuel is a major milestone for the energy transition
RWE is making its power station control system fit for the future by adopting a new technology. Optime, a new SCADA system based on Siemens Spectrum Power, gives RWE a uniform control technology. SCADA stands for 'Supervisory Control and Data Acquisition' – in other words monitoring and managing technical processes using a computer system. Previously, there were two separate systems: one for power plants in Germany and another for the Netherlands and Belgium. The new solution combines the two, while integrating RWE’s renewable energy assets in Europe. It can also accommodate additional units such as battery storage systems and diesel-powered backup generators.