- First order from Asia for HL-class gas turbine
- New power plant with a capacity of more than one gigawatt
- Efficiency rating of more than 63 percent
Siemens will set up a high-efficiency HL-class power island for a new combined cycle power plant (CCPP) in South Korea. This will be the first two state-of-the-art HL-class gas turbines that Siemens will supply to a customer in Asia. The new plant, which will be built in Yeoju, in South Korea’s Gyeonggi Province, will run on regasified liquefied natural gas (LNG) and offer a generating capacity of more than one gigawatt. With a maximum efficiency rating of more than 63 percent the gas turbine will allow the power station to get the most out of the valuable LNG for electricity generation, enabling especially economical and environmentally friendly operation. The customer is South Korean EPC SK Engineering & Construction Co., Ltd., which is constructing the entire plant for the independent power producer Yeoju Energy Services.
At this year’s European Utility Week (EUW) in Paris, Siemens Smart Infrastructure will demonstrate how it is driving energy intelligence across supply and demand. By helping shape the energy ecosystem across buildings, industry and the grid, Siemens is supporting government, cities and businesses with their sustainability goals. The company will focus on four topics that support the energy transition: sustainable grids, smart distribution, the Internet of Energy and grid edge.
A key milestone on the way to independence: Siemens Energy presented its new management team to its employees today. In addition to an Executive Board, the company will have an expanded international management team, the Group Management Committee. Once Siemens Energy becomes a legally separate entity, this team will be instrumental in implementing the company’s strategic approach. “Announcing the management team is a further critical step on the way to becoming an independent company and an energy pure play. It will enable Siemens Energy to further develop its management system and then focus fully on the requirements of its customers and markets,” said Joe Kaeser, President and CEO of Siemens AG.
- Pakistan’s K-Electric awarded Siemens and China’s Harbin Electric International a contract to build a 900-megawatt combined cycle power plant at the Bin Qasim Power Complex in Karachi
- Siemens to supply two F-class gas turbines, steam turbines, generators and condensers
Siemens along with partner Harbin Electric International, signed an agreement with K-Electric to build a 900-megawatt combined cycle power plant at the Bin Qasim Power Complex in Karachi.
- Portfolio serving entire power range from 50 to 600 kW
- Flexible combination with connection options as cable and pantographs
- For fast and secure charging at the depot and en route
- Cloud-based control and monitoring of charging processes
At Busworld 2019, Siemens is presenting its Sicharge UC family for charging electric buses, trucks and duty vehicles at the depot and en route. The Sicharge UC charging system covers the entire power range from 50 to 600 kilowatts (kW) and can be combined with several connection options such as charging plugs and offboard or onboard pantographs. To meet growing demands from the vehicle industry for higher voltages, the station can operate at up to 1,000 volts (V). Electric vehicles with various technologies and batteries can therefore be charged flexibly, either en route or at the depot. The charging processes can be monitored and controlled via a MindSphere application. MindSphere is the cloud-based, open IoT operating system from Siemens.
- Business to be officially renamed as
of April 2020
- Employees’ favorite selected
At an internal management conference, Siemens today announced the name of the new energy company that it is creating. The business, which combines the worlds of conventional and renewable energy and is to become an independent company in the future, is to be called Siemens Energy. The new name will officially take effect once the energy business becomes a separate legal entity, which is expected to happen in April 2020. Siemens Energy is to be spun off as a publicly listed company by September 2020. Its offerings will address a significant portion of the value chain across the oil and gas, power generation, and power transmission segments, including the related service activities. On a pro-forma basis, Siemens Energy generates about €27 billion in revenue and has some 88,000 employees worldwide as well as an order backlog of €70 billion. Today, 20 percent of the world’s energy supply is already based on Siemens technology.
- Power plants Termoeléctrica del Sur, de Warnes, and Entre Ríos inaugurated in August and September
- Upgrade to combined cycle power plants increase the generation capacity by one gigawatt
- Expansion provides reliable energy supply and will allow export of value-added products
With the official inauguration of the Termoeléctrica de Warnes power plant in mid-September, all three power plants in Bolivia were inaugurated within a few weeks in August and September. Since the contract signing in 2016, Siemens has expanded Bolivia’s three largest thermal power plants to efficient combined cycle mode. The power plants are owned and operated by Ende Andina SAM. Together, all three add more than one gigawatt of electrical power to its current maximum capacity and to the Bolivian national grid.
- Latest advances in depot charging for eBuses and eTrucks to be tested in real-life conditions at the “VDL Charging Test Center” in The Netherlands
- Collaboration to demonstrate how vehicle technologies, energy storage and charging systems work together
- Vehicle-to-grid function enables bidirectional charging
- Capacity can be flexibly combined through special switching matrix
As the number of electric vehicles in the market continues to grow, so do the requirements for a robust charging infrastructure. Recognizing the need for electric buses and trucks to be charged flexibly and efficiently, Siemens and VDL Bus & Coach (VDL), a Dutch bus manufacturer, have joined efforts to come up with innovative solutions for depots. At the VDL Charging Test Center Siemens has installed the latest generation of fast charging stations, combined with a battery storage system. The location is VDL’s interoperability test and validation center in Valkenswaard in The Netherlands. A special switching matrix allows to flexibly combine the capacity of the charging stations. The setup is managed via an energy management application running on MindSphere, the cloud-based, open IoT operating system from Siemens. VDL will use this technology to conduct interoperability and function tests on electric vehicles such as buses and trucks. Interoperability is when technologies of different manufacturers – on the vehicle as well as the charging infrastructure side – can interact and exchange information
The new Bauhaus Museum Dessau (Germany) opened its doors in September 2019, featuring technology from Siemens Smart Infrastructure to help keep visitors and its extensive collection safe. A comprehensive solution for safe electrical installations extends throughout the museum’s 5,500 square meter footprint, which includes over 1,000 exhibits from the Bauhaus Dessau Foundation’s collection. The latter comprises 49,000 objects, making it the second-largest Bauhaus collection worldwide. It contains numerous student works and teaching documentation, as well as drafts and prototypes from the workshops of the renowned art academy, which celebrates its 100
th anniversary this year.