- Gas turbine rotor exchange allows for increased output and efficiency
- Control system upgraded to latest version of SPPA-T3000
The Dunamenti Power Plant in Százhalombatta, Hungary, is the largest gas-fired power plant in the country with a capacity of 794 megawatts (MW), making it a major source of reliable electricity in Hungary. Recently, in collaboration with the customer and plant owner, MET Asset Management AG, and within the scope of an overhaul project, Siemens Gas and Power replaced the entire rotor of the plant's SGT5-2000E gas turbine and installed a new, state-of-the-art SPPA-T3000 control system.
- New trend to supply renewable energy for mines as secure and cost-efficient alternative to fossil fuels
-
- Siemens' proven microgrid controller serves as technical basis for juwi's Hybrid IQ microgrid solutions
- Two projects in Australia successfully delivered, paving way for partners to roll-out solution in other countries
Siemens and the renewable energy developer juwi have joined forces to enter into a strategic technology partnership to focus on microgrids in the mining industry. A corresponding agreement was signed today. The two companies aim to roll-out and continually develop the advanced microgrid control system that enables the seamless integration of power from renewable energy to a mine's off-grid power supply. The Siemens Sicam based microgrid control platform is a proven and tested technology which is the basis for juwi's Hybrid IQ microgrid controller. juwi, on the other hand, brings industry-specific domain know-how and an excellent track record of planning and executing renewable energy projects at mine sites.
- Sinamics Startdrive V16 brings a single-axis version of Sinamics S120 to the TIA Portal.
- Innovative functions simplify safety approval, reduce commissioning times and increase user-friendliness.
Sinamics Startdrive commissioning software is the perfect tool for integrating drive hardware into the TIA Portal engineering framework. With the latest version Sinamics Startdrive V16, Siemens is expanding the hardware portfolio available on the automation platform. Following on from the integration of the Sinamics S120 multi-axis system, the single-axis version of this high-end servo drive system can now also be engineered in the TIA Portal. The drive control of the recently introduced Simatic Drive Controller is now also integrated in the commissioning tool. Drive-CliQ hubs, which increase the number of interfaces in the Sinamics S120 multi-axis group, as well as other add-on components, are now integrated in the TIA Portal, perfectly completing this hardware update.
- Designed for future power networks and digital substations
- Enhanced cyber security and communications
- User-friendly interfaces and software
With the new Reyrolle 5 series of protection relays, Siemens is further developing its offerings for medium-voltage and industrial power networks. The protection, control, monitoring and measuring of power networks is a vital element in managing electrical assets, increasing reliability, sustainability and the safety of operating personnel. The first device applications of the new generation of protection relay will be overcurrent and earth fault protection and transformer protection in substations. It includes comprehensive functionality as standard, with enhanced process data such as faults, events and waveform records enabling the power network to be effectively managed. The small number of device variants allows easy ordering and efficient engineering while the improved hardware platform makes it even easier to operate and manage the protection relays.
- Successful collaboration to be showcased at Formnext 2019
- CEAD lightweight extruder to allow high deposition rate and large print volumes mounted on a robot
- Sinumerik Run MyRobot /Direct Control for precise printing with Comau robot and CEAD extruder
CEAD, technology supplier of 3D printing equipment on the frontier of large scale polymer, glass and carbon fibers 3D printing, and Siemens intensify their collaboration and showcase their latest development the AM Flexbot at the upcoming Formnext 2019, a leading trade fair for Additive Manufacturing, on the Siemens booth D81, Hall 12.1.
At this year’s European Utility Week (EUW) in Paris, Siemens Smart Infrastructure will demonstrate how it is driving energy intelligence across supply and demand. By helping shape the energy ecosystem across buildings, industry and the grid, Siemens is supporting government, cities and businesses with their sustainability goals. The company will focus on four topics that support the energy transition: sustainable grids, smart distribution, the Internet of Energy and grid edge.
By 2035, more than 50 percent of electricity is expected to be generated by renewables. In parallel, electricity consumption is forecast to double by 2050. Megatrends such as increasing urbanization and climate change are driving the need for electrification and decarbonization. Meanwhile, new applications in software and digitalization are making grids smarter and more efficient, creating new business models.
- Electrical capacity increased to approximately 1,200 megawatts
- Fired with regasified liquefied natural gas instead of oil
- Fifty percent lower CO2 emissions per kilowatt hour produced
Siemens will provide the equipment to upgrade the Hiep Phuoc 1 steam power plant in Ho Chi Minh City, Vietnam, to a combined cycle power plant. This project will increase the plant’s electrical capacity by roughly 780 megawatts (MW) to approximately 1,200 MW. The modernized plant will be fired with regasified liquefied natural gas (LNG) instead of the oil that has been used to date. By changing the fuel, deploying modern F-class gas turbines from Siemens, and using the waste heat from the gas turbines to produce electricity, the CO2 emissions can be cut almost in half for each kilowatt hour produced on-site. With this project, the customer Hiep Phuoc Power Co. Ltd., will ensure a reliable, secure, and environmentally friendly power supply for Ho Chi Minh City and Vietnam.
- Atlas 3D helps designers define optimal part orientations for ‘right first time’ 3D printing
- Cloud-based, GPU-accelerated Sunata™ software can reduce downstream 3D printing errors caused by thermal distortion up to one hundred times faster than other solutions on the market
Siemens announced today that it has signed an agreement to acquire Atlas 3D, Inc., a Plymouth, Indiana-based developer of software that works with direct metal laser sintering (DMLS) printers to automatically provide design engineers with the optimal print orientation and requisite support structures for additive parts in near real-time. Atlas 3D will join Siemens Digital Industries Software, where its solutions will expand additive manufacturing capabilities in the Xcelerator portfolio of software.
- Company plans enterprise-wide rollout of Siemens Opcenter solutions to streamline production value chain
Siemens Digital Industries Software announced today a collaboration with The Absolut Company regarding Siemens Opcenter™ Execution software, part of the Siemens Digital Enterprise Suite, Manufacturing Execution System (MES) solution. The company will conduct a pilot of Siemens Opcenter Execution Process (formerly known as SIMATIC IT® Unified Architecture Process Industries) in one of their three factories in Åhus as the first step of an enterprise-wide roll-out across the three factories which produce spirits for global distribution. Siemens Opcenter can help The Absolut Company to better meet some of the challenges in beverage market including the increasing demand for high quality and variety in products and production as well as the high cost pressures of the global food and beverage market.
- New Grid Diagnostic Suite offers unique comprehensive insights
- Gain a grid-wide view of energy automation systems
- Market launch of initially four cloud-enabled applications
- Enhances cost efficiency and availability of smart grids
- Support through digitalization in increasingly complex power grids
Siemens is presenting for the first time its new Grid Diagnostic Suite at the European Utility Week in Paris. The Grid Diagnostic Suite initially includes four cloud-based applications which collect data from new or existing field devices for protection, distribution automation and power quality. These data are stored and analyzed in the cloud. This requires almost no additional engineering effort. Distribution grid operators and operators of electricity grids in industrial parks can quickly tap into useful information from devices installed anywhere in the smart grid. This will enable grid faults, for example, to be detected at an early stage and quickly rectified. After information is collected, vulnerabilities can be identified, and necessary measures can be implemented before any damage occurs. In this way, Internet of Things (IoT) applications in the Grid Diagnostic Suite enhance the availability of power grids while enabling them to be operated cost-efficiently.