- Simatic IOT2050 gateway designed for industrial IT solutions directly in the production plant
- Future edge functionality for integration in Siemens Industrial Edge solutions
- Open platform acquires, processes and transfers production data to a cloud system
- Wide range of communication options und easy connection to MindSphere, the open, cloud-based, IoT operating system from Siemens
Siemens is launching a gateway based on the TI ARM processor family which links cloud, in-company IT and production. Simatic IOT2050 is designed for industrial IT solutions for the acquisition, processing and transfer of data directly in the production environment. It can be used for connecting the production process to a cloud-based analysis of machine and production data, for example. The new IOT gateway will also be equipped with remote edge functionality for easy integration into Siemens Industrial Edge solutions.
- Logo! logic module series 8.3 now with direct cloud connectivity
- Guided setup for cloud connection with Logo! Soft Comfort 8.3
- Logo! Web Editor V2.0 with extended functionality
Siemens is presenting the new version of the logic module series Logo! for the first time at Hannover Messe 2020: The latest Logo! Version 8.3 will be available from Fall 2020 and features a direct cloud connection. The Logo! Soft Comfort engineering software is getting a functional update to enable configuration of the new devices. With Version 8.3, it is possible to activate and configure the cloud connection and use the new free Logo! web editor to create user-defined website and dashboards in the cloud. Users can also design their automation projects and operate them from the cloud via smartphone, tablet or PC. The webserver can be directly hosted in the cloud, enabling individual visualization and centralized control of switching and automation solutions in building management systems, and in the construction of control cabinets, machines and apparatus – comfortably, regardless of the location. Users now have even more options for simple networking.
- Siemens’ Xcelerator portfolio will help support BYD in their
transformation to a digital enterprise
Siemens Digital Industries Software
announces a strategic partnership with BYD, a Chinese manufacturer and leader
in the automotive and new energy industries. With this partnership, BYD plans
to build a digital enterprise strategy using the full scope of Siemens’
solutions. Using these solutions, BYD will be able to use digital twins to provide
detailed insight into all aspects of decision-making for product development
and production operations. By connecting these digital twins with a consistent
digital thread, BYD can realize the power and flexibility to speed up
development, optimize manufacturing and use the insight gained from product and
plant operations to improve future performance.
- Siemens’ MindSphere Named an Industrial IoT Software Platforms Leader by Independent Research Firm
- Partner ecosystem now includes SAS, AWS, Microsoft, Alibaba and Arrow Electronics
- MindSphere extends Xcelerator portfolio to enable tomorrow’s engineering, today
The Industrial Internet of Things (IIoT) has the potential to significantly improve global productivity and growth, with Accenture estimating that this latest wave of digital innovation will accelerate the reinvention of sectors that account for almost two-thirds of world output and add US$14.2 trillion to the global economy by 2030. As companies around the world continue to develop IIoT strategies and implement solutions, they are increasingly partnering with Siemens and choosing MindSphere®, the cloud-based, open Internet of Things (IoT) operating system, as the foundation of their IIoT programs. Recently, Siemens was among the select companies that Forrester invited to participate in The Forrester Wave™: Industrial IoT Software Platforms, Q4 2019 evaluation. In this evaluation, Siemens’ MindSphere was cited as a Leader in Industrial IoT Software Platforms. Over the past year, MindSphere significantly grew its partner program, and announced major new customer wins and Siemens’ expansion of the Mendix platform to include cloud and app services for digital engineering and IoT powered by MindSphere, which is at the heart of its powerful Xcelerator portfolio.
- Siemens' Capital is selected by Europe's second largest car
manufacturer to automatically render electrical system diagrams, replacing
manual processes
- Accurate documentation helps ensure rapid and effective vehicle
maintenance, helping Groupe PSA realize a 30% schedule reduction
- Capital
is part of the Xcelerator portfolio of software, which is enabling tomorrow's
electronic design today
Siemens today announced that Siemens'
Capital™ software
electrical design product for
its automotive aftersales documentation has been selected by Groupe PSA
, the second largest car manufacturer in Europe. Groupe PSA is an early
innovator of autonomous and connected cars, manufacturing five car brands:
Peugeot, Citroën, DS, Opel and Vauxhall. The company has an established process
of supplying its facilities with after-sales service documentation with several
types of design deliverables aiding rapid diagnosis. Using Capital's advanced
technology, Groupe PSA has replaced a largely manual process and can now
automatically render their electrical system diagrams using data that comes
directly from the PSA electrical/electronic (E/E) engineering department and
their harness suppliers to help provide "correct-by-construction" assurance.
The result is accurate documentation created using "as-manufactured"
data provided by Groupe PSA's suppliers which helps ensure rapid and effective vehicle
maintenance when required. Groupe PSA can now better enable their digital
enterprise and continue to innovate the mobile solutions of the future.
- Fast 1,000 Hz sampling rate and processing time deliver high accuracy and repeatability
- Seamless, user-friendly integration into Simatic automation systems
- Wide range of applications in pharmaceutical, food and beverage, chemical, and steel industries
Siwarex WP351 is Siemens’ newest solution for intelligent weighing automation. Measuring 20 millimeters width by 65 millimeters height, the module is one of the smallest weighing electronics units available. The device’s 1,000 Hz sampling rate and processing time combined with a digital output response time of less than one millisecond guarantee highest accuracy and repeatability. This capability represents especially in case of checking scales and high performance filling machines a big advantage, as even within very short weighing times the dosing devices are controlled in an optimal way.
- Guided acceptance test for safety functions in the Sinamics Startdrive engineering tool
- Extremely user-friendly thanks to acceptance wizard
- Automatically generated and standard-compliant acceptance report supports documentation
With Sinamics Startdrive commissioning software, Siemens supports machine builders in the validation of safety functions for Sinamics frequency converters with a guided acceptance test. With Sinamics Startdrive, Siemens offers a tool for the integration of drive hardware into the TIA Portal engineering framework. The integrated guided acceptance test for safety functions is available for Sinamics G and S series frequency converters and complies with EN ISO 13849-2 and IEC 62061.
- Seamless redundancy and high precision time synchronization from a single device
- Easy migration to highly reliable networks with zero packet loss
- Minimal downtime and reduced risk of communication disruptions
- Specifically designed for modern digital substation applications
Siemens has introduced a new line module for the Ruggedcom RST2228 and RST2228P Layer 2 19” rack switches, the Ruggedcom RMM2972-2RNA. This module strengthens the Ruggedcom RST2228 19” rack switch offering to the electric power utilities by providing seamless redundancy with PRP/HSR (Parallel Redundancy Protocol/High-availability Seamless Redundancy), enhanced IEEE1588 implementation, high bandwidth uplinks, and traffic filtering and segmentation from a single device. This module eliminates network downtime due to single points of fault, resulting in high reliability and availability for modern digital substation applications as mandated by the IEC 61850 standard.
- Partnership brings together leading-edge integrated circuit (IC) methodologies, processes and tools to help the automotive supply chain solve design and verification challenges
- Leveraging Arm automotive IP and software within Siemens’ PAVE360 digital twin environment enables collaboration and empowers automakers and suppliers to develop and validate differentiated safety enabled systems, ICs and software solutions in the context of the entire vehicle
- Siemens’ PAVE360, part of Siemens Digital Industries Software’s Xcelerator portfolio, helps automotive companies innovate and develop the complex electronic systems needed for today and tomorrow’s vehicles
Siemens Digital Industries Software today announced a partnership with global semiconductor IP leader Arm, that will bring leading edge IP, methodologies, processes and tools together to help automakers, integrators and suppliers collaborate, design and bring to market their next-generation platforms much faster. This partnership was formed to address the increasingly complex challenges facing the industry in developing platforms to realize active-safety, advanced driver assistance, in-vehicle infotainment, digital cockpits, vehicle-to-vehicle/vehicle-to-infrastructure and self-driving vehicles. Key advances in computing and sensor technology are enabling companies to redefine mobility beginning with the integrated circuits and software within automotive electronics systems. The combination of Siemens’ and Arm’s innovative technologies can help automakers and suppliers deliver tomorrow’s electronic design and automotive solutions, today.
- Voltage variant of Sinamics G120X for USA and Latin America
- Save space with new size for the Sinamics V20
- Adapter kit to physically and thermally separate power module and control unit for Sinamics G120
With numerous innovations, Siemens is extending its drive portfolio, improving user-friendliness and offering space-saving installation options. The Sinamics G120X converter, designed specifically for use in water/wastewater applications and in HVAC systems, is now also available in a three-phase 3AC 200V voltage variant in the power range up to 55 kW. This means that the converters can now be integrated seamlessly into applications in the USA and in Latin America. Due to its robust construction and the coating of the PCBs according to 3C3 standard the converter is suitable for harsh environments. The new module for extending the digital and analog inputs and outputs increases the flexibility and the optimal control of converter-guided applications. The Sinamics G120X now also supports the communication protocols Profibus, Modbus RTU, USS and BACnet MS/TP. It is equipped with extensive interfaces and can be easily integrated into existing or new systems.