- Siemens expands long-standing relationship supporting U.S. Air Force with proven digital capabilities to innovate in the defense industry
Siemens today announced the U.S. Air Force has selected
Teamcenter® software as the foundational system of record to support its digital acquisition and sustainment strategy for critical systems and technologies across the service. The selection of Teamcenter as the Air Force enterprise standard follows a 2019 indefinite-delivery / indefinite-quantity contract for $24.6 million to Siemens for licensing, maintenance and support.
- Voltage
range up to 1,000 V and scalable charging power up to 300 kW
- High
efficiency for reduced operational cost at high power flow
- Automated allocation and shifting of charging power
Siemens
Smart Infrastructure released its new public fast charger Sicharge D for the IEC markets. It is suited
for highway and urban fast charging stations, city parking as well as shopping
malls and provides one of highest peak efficiencies on the market at 96 percent,
scalable charging power and dynamic power sharing.
- Monte Rosa Hut in Swiss Alps modernized with new battery storage solution
- Solar power ensures sustainable, efficient energy supply
- 8.6 tons of lead batteries replaced with 2.7 tons of lithium batteries
The “Bergkristall” (Mountain Crystal), a mountain hut situated at an altitude of 2,883 meters in the Monte Rosa Massif of the Valais Alps, has been largely energy self-sufficient since 2010. Along with thermal solar collectors, a photovoltaic system integrated in the hut’s southern facade ensures a high degree of energy self-sufficiency and a reliable energy supply. Since 2010, all of the building’s performance data, such as solar energy generated and battery capacity, have been bundled in Siemens Navigator, the cloud-based building performance platform.
- One single device for lines of up to 500 km
- Monitoring for powered, unpowered or grounded lines
- Highly precise localization of line faults
- Simplifies maintenance and increases network reliability
Siemens Smart Infrastructure recently launched its new PowerLink CM, a condition monitoring solution for high-voltage AC and DC transmission lines. To ensure reliable power supply, optimize grid utilization and prevent blackouts the device is designed to precisely locate faults in the transmission grid and continuously track line conditions. One single PowerLink CM device is sufficient to monitor line lengths of up to 500 km. Faults as well as line condition can be detected in powered, unpowered or grounded lines. Fault reports are received by the affected substation and are forwarded from there to the control room. For continuous line monitoring, the device can be connected to MindSphere, the open cloud-based Internet of Things (IoT) platform from Siemens, which facilitates transparent processing of all line data in the cloud. This allows grid operators to analyze status reports and optimize maintenance activities.
- Charging, medium and low-voltage technology for two carports at Hamburger Hochbahn AG’s Alsterdorf bus depot
- Space-saving installation as technical center on carport’s roof
- Important step for transitioning to climate-friendly local transport in Hamburg
Siemens Smart Infrastructure won a major contract from Hamburger Hochbahn, the largest local transport provider in the Hanseatic city. Siemens will equip two of the six carports at the Alsterdorf bus depot with a total of 96 charging points as well as medium and low-voltage technology. Operations are scheduled to start in summer 2021. With a total of 240 parking spaces, it is one of the largest and most modern bus depots for electric buses in Europe.
- FIA and Siemens extend partnership to provide the ‘FIA Mobility Advocate’— a unique software and hardware toolkit — for FIA Mobility Member Clubs to strengthen advocacy of future transport solutions
As an
“Official Supplier of Urban Mobility Advocacy Solutions” for the Fédération Internationale de l’Automobile (FIA), the governing body of world motor sport and
the federation of the world's leading motoring organisations, Siemens plans to
develop a toolkit of software solutions for FIA Member Clubs to help them
provide an evidence-based approach to advocate for the implementation of mobility
policies and strategies. The ‘FIA Mobility Advocate’ combines modeling for
mobility, autonomous vehicles, and the environment, with enhanced analysis
outputs to help meet current future mobility goals.
- Sitrans CC240 IOT gateway provides standardized access to the lifecycle data of HART® devices
- Reduced service effort thanks to faster identification and removal of measuring and parameterization errors without additional parameterization tools
- Compatible with all OPC UA client applications
- Direct connection to Siemens MindSphere
- Numerous possible applications for on and off-premise solutions
Siemens presents the Sitrans CloudConnect 240: a new IOT gateway for the process industry. It provides a second data channel, completely independent of the control system, which is used to transmit data from any HART®-based field devices to the IT world.
- Siemens and Hassan Allam Construction to build new control center located in Egypt’s New Administrative Capital
- Customer is Egyptian Electricity Transmission Company
- Latest software to monitor, manage and control extra-high voltage transmission networks and power generation plants across the country
- Contract worth more than EUR 45 Mio.
Egyptian Electricity Transmission Company has awarded a contract to the consortium consisting of Siemens Smart Infrastructure and Hassan Allam Construction to build the new National Energy Control Center in the New Administrative Capital of Egypt. The country’s new power grid control center will deploy advanced software and equipment to monitor, manage and control extra-high voltage (220 kV and 500 kV) transmission networks and power generation stations across Egypt. The necessary technologies will be included in the new control center for future grid expansion while maintaining secure energy supply, including intermittent renewable energy sources and storage. The project is expected to be completed by the end of 2022.
- Closed system operation for patients and medical personnel’s safety
- Contamination protection with flexible, scalable HVAC control solution
- Compliant with healthcare industry standards
- Easy installation and operation from anywhere
Siemens Smart Infrastructure (SI) has teamed up with Auto-Info to jointly develop a modular COVID-19 examination unit. The mobile lab structure and system have been designed to avoid contamination among patients or from patients to medical staff by using the Climatix IC platform, a flexible and scalable advanced HVAC control solution from Siemens.
-
White Space Cooling Optimization for highly efficient greenfield data center in Paris region
- Intelligent, continuously learning solution to support data center’s 24/7 availability and energy efficiency
Siemens Smart Infrastructure is supplying the first Tier IV-certified data center in the region of Paris, France. The “Thésée” data center will meet the highest industry standards for availability and energy efficiency. Siemens will install its White Space Cooling Optimization (WSCO) smart solution to optimize the building’s energy efficiency as well as the thermal protection of the server rooms by automatically adjusting the operation of the cooling systems.