- First soft starter series with integrated Safe Torque Off function
- Enhanced protection when shutting down electric motors
- High functional density saves space and decreases cost
Siemens Smart Infrastructure expanded its soft starters portfolio for motors, with the launch of Sirius 3RW55 Failsafe and Sirius 3RW50. Soft starters ensure electrical motors used in industry and infrastructure are protected during startup and ramp-down. The Sirius 3RW55 Failsafe soft starters are the first to feature the integrated Safe Torque Off (STO) function. As specified in safety standards, the protection function for electrical drive systems ensures that torque-generating energy stops acting when motors are turned off, preventing an unwanted restart. Control panel manufacturers no longer require using separate individual components to have this function, which reduces the time and effort for wiring and maintenance works and saves space in the control cabinet. In addition, the switching time of the integrated solution is significantly shorter than for conventional, electromechanical components.
- New Simotics HV M slipring motors provide range of power up to 4.5 MW
- Easy integration into SIDRIVE IQ applications for highest availability, serviceability, productivity and efficiency
- Easy plant integration due to 3-D Motor models to speed up complete plant integration processes
- Certified and proven Siemens MICALASTIC® VPI insulation system with extreme long lifetime
Building on more than a century of experience in manufacturing slipring motors, Siemens today announces the new Simotics HV M slipring motor. Designed and engineered for applications mainly in the cement and mining industries, the newest slipring motor is implemented in a wide range of applications including but not limited to mills, crushers, conveyors and fans. The new platform motor with its power range up to 4.5 MW completes the Siemens slipring motor family which covers now the power range from 0.5 to 8.2 MW.
At this year’s European Utility Week (EUW) in Paris, Siemens Smart Infrastructure will demonstrate how it is driving energy intelligence across supply and demand. By helping shape the energy ecosystem across buildings, industry and the grid, Siemens is supporting government, cities and businesses with their sustainability goals. The company will focus on four topics that support the energy transition: sustainable grids, smart distribution, the Internet of Energy and grid edge.
- Portfolio serving entire power range from 50 to 600 kW
- Flexible combination with connection options as cable and pantographs
- For fast and secure charging at the depot and en route
- Cloud-based control and monitoring of charging processes
At Busworld 2019, Siemens is presenting its Sicharge UC family for charging electric buses, trucks and duty vehicles at the depot and en route. The Sicharge UC charging system covers the entire power range from 50 to 600 kilowatts (kW) and can be combined with several connection options such as charging plugs and offboard or onboard pantographs. To meet growing demands from the vehicle industry for higher voltages, the station can operate at up to 1,000 volts (V). Electric vehicles with various technologies and batteries can therefore be charged flexibly, either en route or at the depot. The charging processes can be monitored and controlled via a MindSphere application. MindSphere is the cloud-based, open IoT operating system from Siemens.
- Conveyor system will move 127,500 tons of primary crushed ore per day
- New Siemens’ gearless drive technology to increase reliability and efficiency additionally by up to 4 percent
- Maintenance requirements of the drive system significantly reduced
Powered by Siemens’ new gearless drive technology, thyssenkrupp’s high-capacity overland conveyor will access one of the world’s largest copper reserves in Quellaveco. The Quellaveco mine in Peru contains approximately 7.5 million tons of copper in ore reserves – enough to wire 80 million homes or equip 90 million electric vehicles.
- Latest advances in depot charging for eBuses and eTrucks to be tested in real-life conditions at the “VDL Charging Test Center” in The Netherlands
- Collaboration to demonstrate how vehicle technologies, energy storage and charging systems work together
- Vehicle-to-grid function enables bidirectional charging
- Capacity can be flexibly combined through special switching matrix
As the number of electric vehicles in the market continues to grow, so do the requirements for a robust charging infrastructure. Recognizing the need for electric buses and trucks to be charged flexibly and efficiently, Siemens and VDL Bus & Coach (VDL), a Dutch bus manufacturer, have joined efforts to come up with innovative solutions for depots. At the VDL Charging Test Center Siemens has installed the latest generation of fast charging stations, combined with a battery storage system. The location is VDL’s interoperability test and validation center in Valkenswaard in The Netherlands. A special switching matrix allows to flexibly combine the capacity of the charging stations. The setup is managed via an energy management application running on MindSphere, the cloud-based, open IoT operating system from Siemens. VDL will use this technology to conduct interoperability and function tests on electric vehicles such as buses and trucks. Interoperability is when technologies of different manufacturers – on the vehicle as well as the charging infrastructure side – can interact and exchange information
The new Bauhaus Museum Dessau (Germany) opened its doors in September 2019, featuring technology from Siemens Smart Infrastructure to help keep visitors and its extensive collection safe. A comprehensive solution for safe electrical installations extends throughout the museum’s 5,500 square meter footprint, which includes over 1,000 exhibits from the Bauhaus Dessau Foundation’s collection. The latter comprises 49,000 objects, making it the second-largest Bauhaus collection worldwide. It contains numerous student works and teaching documentation, as well as drafts and prototypes from the workshops of the renowned art academy, which celebrates its 100
th anniversary this year.
- Automatic handling of up to 1800 pieces of luggage per hour
- Improved security and more comfort for travelers and airport staff
- Modernization in compliance with tightened international security rules for luggage inspection
- Siemens also providing management systems, software and communications for remote operation
- Order volume of 164 million euros
Siemens will modernize the existing security systems for luggage control at Spain's five busiest airports. The contract for the luggage inspection systems at the airports of Madrid, Barcelona, Malaga, Palma de Mallorca and Gran Canaria has a volume of around 164 million euros. The customer is AENA (Aeropuertos Españoles y Navegación Aérea), the Spanish semi-governmental airport operator. With 264 million passengers and more than one million tons of freight in 2018, AENA is one of the world's largest airport operators. The new luggage inspection systems from Siemens will help to significantly increase traveler safety. At the same time, passengers can be handled more quickly and travel more comfortably.
- Retrofit of substation automation and protection system in Norway including Internet of Things (IoT) connectivity
- Consolidation, visualization and analysis of grid data in MindSphere cloud
- Option to develop additional use cases during project execution
- Digitalization of grid assets optimizes overall efficiency
Together with the Norwegian distribution system operator Glitre Energi Nett, Siemens will build a digital substation to pilot Internet of things (IoT) analytics and applications for power grids. IoT-ready Siprotec protection and control and Sicam automation devices will be connected via OPC UA PubSub, an open standard communication protocol, to MindSphere – the Siemens cloud-based open operating system for IoT. The Siprotec dashboard cloud application will make previously inaccessible data fully available and help to process grid data for the first time in the cloud with zero engineering effort.
Let the good times roll: Starting September 21, about six million people from all around the world will be enjoying themselves at the Oktoberfest in Munich for two weeks. Traditionally, Siemens supplies drives and control systems as well as energy distribution for the festival's rides. Automation solutions from Siemens also control special beer pipelines – the only ones of its kind worldwide –that supply the Hacker, Winzerer Faehndl and Braeurosl festival tents with their tasty Oktoberfest brews. Because many breweries use Siemens technologies within their brewing process, Siemens doesn't only ensure fresh beer at the Oktoberfest.