- Siemens will refurbish 30-year-old HVDC back-to-back system in the State of Madhya Pradesh in India
- Modernization will extend the lifetime to ensure reliable power supply
- First Siemens refurbishment project of a third-party HVDC system
Power Grid Corporation of India (POWERGRID), the Central Transmission Utility of India, has chosen Siemens to modernize the country's first and oldest high voltage direct current (HVDC) link, Vindhyachal. Located in the central Indian state of Madhya Pradesh, the 500-megawatt HVDC back-to-back system was put into operation in 1989 to interconnect the asynchronous 400-kilovolt alternating current networks of the Northern and Western regions. By installing its latest HVDC components Siemens will extend the useful life of the link. This will be the first Siemens HVDC modernization project in India and globally the company's first refurbishment of a third-party system involving replacement of the thyristor valves. The upgrade is expected to be completed in 2021.
Arja Talakar has been appointed CEO of Siemens Oil & Gas, effective April 1, 2019. He will be based in Houston, Texas, the global headquarters for Oil & Gas and its parent operating company, Siemens Gas and Power.
- Siemens will supply three Dresser-Rand® 5HHE-VL-3NL reciprocating compressors for what will become the largest hydrogen production unit in the United States.
A leading industrial gas company recently selected Siemens to supply three Dresser-Rand® 5HHE-VL-NL reciprocating compressors for a new, state-of-the-art steam methane reformer (SMR) in Texas. The SMR will provide high-purity hydrogen for the gas company’s customers throughout the region.
- Siemens' broad energy portfolio and services will help ensure long-term reliability and efficient operations
- Integrated, redundant plant design features two SGT-600 gas turbines with DLE technology running on residue gas with high concentrations of hydrogen
- Project highlights the integrated value of Siemens Gas and Power
Braskem, the largest petrochemical company in Latin America, recently entered into an agreement with Siemens to modernize a cogeneration power and steam plant at its Petrochemical Complex in Sao Paulo, Brazil. Completion of the project is expected in early 2021.
- 1.3-gigawatt turnkey combined cycle power plant
- Long-term service program and operation & maintenance (O&M) services included
- Largest LNG-to-power development in Latin America
- Total project volume of €1 billion
Siemens has secured an order for the turnkey construction of a new combined cycle power plant for the integrated LNG-to-Power project GNA 1 of Gás Natural Açu in the Port of Açu in the state of Rio de Janeiro, Brazil. Siemens is providing an equity investment and owns one-third of the project company Gás Natural Açu (GNA) together with Brazil logistics company Prumo Logística S.A. and BP. In addition, Siemens signed a long-term service agreement and will operate and maintain the plant to help ensure reliability, availability and operational performance. The order is the first application for the highly efficient and proven Siemens H-class gas turbine in Brazil. With a capacity of approximately 1.3 gigawatts (GW), the power plant will provide affordable and clean energy for Brazil. Total project volume for GNA 1 is approximately €1 billion (R$4.5 billion).
- SensgearTM technology launch for digital connectivity of switchgear products
- New Sensformer® advanced with applications based on digital twin simulation of transformers
- Portfolio extension comes with comprehensive data analytics for added transparency, enhanced productivity, and advanced intelligence
Siemens is introducing Sensgear, its new digital switchgear portfolio, and the Sensformer advanced at this year's Hannover Messe. With the combination of the already well-established digitally connected transformer, the Sensformer, and the new Sensgear technology, all substation transmission assets are now fully connective, allowing operators to check their status via online applications in real time. Gas-insulated switchgear, circuit breakers, surge arresters, disconnectors, instrument transformers, and coil products will henceforth be equipped with Sensgear technology. All devices are connected via a smart and robust Internet of Things (IoT) gateway that securely transmits the required information to a cloud-based storage and visualization platform. All Sensgear products provide additional transparency with GPS and local weather information as well as product-specific measurement data that includes gas density, liquid temperature, gas leakage, and switching position.
- Services support first use of Siemens H-class turbine in an aluminum smelting facility globally
- Siemens' first long-term service agreement in the UAE for an H-class turbine
- Power services will ensure reliable operations for stable power production
Emirates Global Aluminum (EGA), the world's largest 'premium aluminum' producer, and Siemens announced the first power services agreement for an H-class gas turbine in the United Arab Emirates (UAE). With the new 20-year service agreement, Siemens will provide maintenance and repairs as well as onsite personnel support for the gas turbine and its generator at the planned over 600-megawatt (MW) combined cycle project feeding EGA's Jebel Ali power plant in Dubai.
- Siemens to supply 19 net-gas, off-gas and recycle gas compressors for crude flexibility project
- The project will enable the refinery to process up to 420,000 barrels per day of offshore crude oil
Siemens was recently selected to provide 19 process reciprocating compressors for ADNOC Refining’s crude flexibility project at Ruwais Refinery-West. The project is intended to increase the refinery’s crude processing flexibility, enabling the site to process up to 420,000 barrels of oil per day of the local crude grade known as Upper Zakum, which is found offshore. The upgrade will improve the value of each barrel of oil and allow ADNOC to export more of its main onshore, lighter-grade Murban crude.
- Fulcrum's municipal solid waste-to-fuels plant will contribute to a sustainable future
Abengoa, a Spanish engineering, procurement and construction (EPC) contractor, recently selected Siemens to supply a compressor train for Fulcrum BioEnergy's Sierra BioFuels Plant that will use gasification technology to produce low-carbon fuels from municipal solid waste. The plant will be located in Storey County outside of Reno Nevada and is expected to produce approximately 11 million gallons of biofuel per year that will be used by the aviation industry.
- Heat and power for the Rhine-Ruhr metropolitan region
- Fuel efficiency exceeding 85 percent
- Long-term service agreement
Siemens and STEAG GuD Herne GmbH signed an agreement today on the turnkey construction of a combined cycle power plant with district heat extraction. They also entered into a long-term service agreement. The Herne 6 plant will have an electrical capacity of more than 600 megawatts (MW). Steam will also be extracted, and the thermal energy obtained will be used for the district heating grid of Germany's Rhine-Ruhr metropolitan region. Never before has a single power plant unit been able to provide 400 MW of (thermal) district heat with combined cycle operation. The overall fuel efficiency of the natural gas used thus climbs to more than 85 percent, making the power plant one of the world's most efficient and most environmentally friendly plants. The investment volume for Herne 6 is in the mid-triple-digit euro range.