Challenges and opportunities in the energy systems require a new smart, more adaptable grid infrastructure. Today, power grid operation is a complex task: Volatile power generation and multi-directional power flows from distributed, increasingly renewable sources and prosumers call for a smarter approach. With digital solutions that connect the physical and digital worlds we integrate intelligence across the energy value chain in systems and operations. We help connect grids, buildings, and industries enhancing efficiency and sustainability. We shape grids that are reliable and resilient, that integrate and manage renewables and that operate increasingly autonomous. These responsive grids support the sustainable energy transition, help provide affordable energy to society and our customers to stay competitive in an ever changing world. During Europe´s largest energy related trade show Enlit, which took place in Milan, Italy, Siemens presented its technological solutions to these challenges.
Cities account for roughly 80 percent of the energy consumed worldwide and generate roughly 75 percent of all carbon emissions. With more than two-thirds of the world’s population predicted to live in urban areas by 2050, cities are coming under increasing pressure. Digitally connected smart cities can help overcome some of the most pressing challenges of our time, including clean water, adequate waste removal as well as reduced pollution caused by buildings. The Expo 2020 Dubai site, with infrastructure connected by Siemens digital technology, provides a blueprint for smart cities globally. As the Premier Partner for Infrastructure Digitalization at Expo 2020 Dubai, Siemens has digitally linked more than 130 buildings at a purpose-built site twice the size of Monaco.
Fluorine gas-free energy distribution for medium-voltage applications
Fluorine gas-free switchgear is a hot topic in the energy sector because this new approach contributes to sustainable power distribution. On this page you will find all information about the sustainable switchgear portfolio from Siemens.
Every plant or asset is documented in data. All this data and information is scattered across various platforms and various formats. It is not contextualized nor is it easily accessible. It is simply not data you can rely on. That is where PlantSight comes in. PlantSight consolidates the assets of a plant, by bringing together different types of data (1D, 2D, or 3D) from different sources into a single source of truth.
Control rooms of process engineering plants are usually
as old as the plant itself, often 30 years and more. Today, digital
transformation is placing new demands on automation: Simatic PCS neo is a brand-new system software, which
offers companies in the process industry unique opportunities in the age of
digitalization. Main features include global web-based collaboration in
engineering and operation and intuitive handling representing all relevant
information in a single workbench.
Let the good times roll: Starting September 21, about six million people from all around the world will be enjoying themselves at the Oktoberfest in Munich for two weeks. Traditionally, Siemens supplies drives and control systems as well as energy distribution for the festival's rides. Automation solutions from Siemens also control special beer pipelines – the only ones of its kind worldwide –that supply the Hacker, Winzerer Faehndl and Braeurosl festival tents with their tasty Oktoberfest brews. Because many breweries use Siemens technologies within their brewing process, Siemens doesn't only ensure fresh beer at the Oktoberfest.
The Siemens Zug campus features a new office building with 1,000 work spaces and a newly constructed production building. The Siemens Zug campus is one of the first new projects to use Building Information Modeling (BIM) for design and construction. The campus complex is equipped with building automation, security and fire safety technology from Siemens BT and particular emphasis was placed on sustainability and energy efficiency of the buildings.
The need for electromobility is growing, as is the need for an efficient charging infrastructure. As a pioneer in electromobility, Siemens has global experience, maintains a strong portfolio along the entire value chain, and plays an active role in advancing the development and standardization of charging solutions worldwide.Siemens is part of the "FastCharge" research project together with BMW Group as consortium leader, Allego GmbH, Phoenix Contact E-Mobility GmbH as well as Dr. Ing. h.c. F. Porsche AG. This project is investigating the technological requirements that vehicles and infrastructure must meet in order to be able to use extremely high charging capacities. The industrial companies involved in the research project presented the latest advancements in the field of fast and convenient energy supply for electrically powered vehicles on December 12, 2018. The prototype of a charging station with a capacity of up to 450 kW was inaugurated in Jettingen-Scheppach, Bavaria. At this ultra-fast charging station, electrically powered research vehicles created as part of the project are able to demonstrate charging times of less than three minutes for the first 100 kilometres of range or 15 minutes for a full charge (10-80 % State of Charge (SOC)).The energy supply system of Siemens used in the project contains both high-power electronics for the charging connections as well as the communication interface to the electric vehicles. For the connection to the public power grid, a charging container was implemented with two charging connections for CCS-compatible vehicles. One connection has an unprecedented charging capacity of max. 450 kW while the second can deliver up to 175 kW.
- Siemens successfully completed the first phase of its shallow water test of the Subsea Power Grid.
- The development program was conducted in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge.
- This will be the world's first Subsea Power Grid for medium voltage power distribution using pressure compensated technology.
Siemens has successfully concluded the first phase of its Subsea Power Grid shallow water test in Trondheim, Norway. Siemens, in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge, is in the final stages of a program to develop a barrier-breaking system that will become the world’s first Subsea Power Grid designed for distribution of medium voltage power using pressure compensated technology.
With the DynaGridCenter project, Siemens worked alongside partners in science and research to develop the next generation of grid control centers. For the first time, assistant systems visualize dynamic processes that bring the energy transition to the power grid and provide targeted recommendations for actions to optimize the grids and prevent blackouts.