- Guided acceptance test for safety functions in the Sinamics Startdrive engineering tool
- Extremely user-friendly thanks to acceptance wizard
- Automatically generated and standard-compliant acceptance report supports documentation
With Sinamics Startdrive commissioning software, Siemens supports machine builders in the validation of safety functions for Sinamics frequency converters with a guided acceptance test. With Sinamics Startdrive, Siemens offers a tool for the integration of drive hardware into the TIA Portal engineering framework. The integrated guided acceptance test for safety functions is available for Sinamics G and S series frequency converters and complies with EN ISO 13849-2 and IEC 62061.
- Siemens Arts Program to showcase
work of persecuted and “ostracized” Jewish musicians in order to mark 75th
anniversary of liberation of Auschwitz concentration camp
- Composer Viktor Ullmann
(1898-1944), murdered in Auschwitz, to be honored with new
3D recording to be released on January 31
- Ullmann’s Piano Concerto Opus 25
recorded for first time in 3D audio format by Rundfunk-Sinfonieorchester
Berlin and Annika Treutler (piano) under the direction of Stephan Frucht
The
Siemens Arts Program has teamed up with pianist Annika Treutler to produce a
new recording of Viktor Ullmann’s Piano Concerto Opus 25, composed in 1939.
This is the first time the work has been recorded using 3D audio processing.
The recording was produced in cooperation with the German broadcaster Deutschlandfunk Kultur and the Rundfunk-Sinfonieorchester Berlin at Berlin-Brandenburg
Broadcasting’s large studio in Berlin under the direction of Stephan Frucht (Artistic Director of the Siemens Arts Program). The recording
process was directed by Professor Thorsten Weigelt (Berlin University of Fine
Arts) and the 3D immersive audio specialist Stefan Bock (IAN Munich).
- Acquisition to address rising demand for low-voltage power distribution in India
- Siemens to acquire 99% of C&S Electric Limited
- Transaction strengthens local market presence, enables creation of export hub
- Closing subject to regulatory approvals
In a step to meet the increasing demand for electrification across industry, infrastructure and buildings in India, Siemens Ltd. (India) today signed an agreement to acquire New Delhi-based C&S Electric Limited. The acquisition of one of the leading providers of electrical and electronic equipment for infrastructure, power generation, transmission and distribution, will strengthen Siemens’ position as a key supplier of low-voltage power distribution and electrical installation technology in one of the world’s fastest-growing economies. Under the agreement, Siemens Ltd. will acquire approximately 99 percent of the equity share capital of C&S Electric Limited for around EUR 267 million (INR 21 billion). Closing of the acquisition is subject to regulatory approvals. In the future, Siemens envisions this partnership to pave the way for the establishment of a design and manufacturing hub in India, supporting the export of electrification solutions to fast-developing markets around the world. Siemens Ltd. is the local, publicly-listed entity of Siemens AG.
To whom it may concern,
First of all, I do want to thank you for the countless
mails, social media engagements and personal meetings over this important matter.
The vast majority has been addressing their concerns clearly and with respect.
For me, this only underscored the importance and the need to diligently look
into the issue at hand. Especially, the messages I’ve received from Australian
people have moved me personally, when they described that their homes and their
country is burning and suffering from these terrible fires.
Even though we do not have clear evidence that the wildfires
and this project are directly connected, I feel empathy for all those, who
spoke up and warned about worsening conditions. Siemens, as one of the first companies
to have pledged carbon neutrality by 2030, fundamentally shares the goal of
making fossil fuels redundant to our economies over time.
The
historical Siemensstadt will be transformed into a new working and living
environment. With Siemensstadt2, Siemens is planning to implement the largest
development project in its history.
- Jury’s decision for design by Berlin firm unanimous
- Clear urban development concept and new high-rise structure in center of Siemensstadt
- Historic location to be successfully transformed for the future
Siemens and the State of Berlin invited 18 architecture firms and urban planning teams to participate in the competition to redesign Siemensstadt (“Siemens City”), the company’s historic location in Berlin. After two days evaluating their proposals, the high-caliber jury has now reached a decision: “Siemensstadt 2.0 will be implemented on the basis of a design submitted by the Berlin firm Ortner & Ortner Baukunst,” said Stefan Behnisch, the distinguished architect who chaired the jury’s deliberations. “In the jury’s view, this design will provide a solid basis for the structure of the future Siemensstadt. It’s not the complete picture. It leaves room for necessary developments. It’s a design that treats the historical buildings with respect while enabling their up-to-date utilization. The design fulfills virtually all today’s requirements, but also leaves room for the future development of a new, modern city where people can both work and live,” he added.
- Seamless redundancy and high precision time synchronization from a single device
- Easy migration to highly reliable networks with zero packet loss
- Minimal downtime and reduced risk of communication disruptions
- Specifically designed for modern digital substation applications
Siemens has introduced a new line module for the Ruggedcom RST2228 and RST2228P Layer 2 19” rack switches, the Ruggedcom RMM2972-2RNA. This module strengthens the Ruggedcom RST2228 19” rack switch offering to the electric power utilities by providing seamless redundancy with PRP/HSR (Parallel Redundancy Protocol/High-availability Seamless Redundancy), enhanced IEEE1588 implementation, high bandwidth uplinks, and traffic filtering and segmentation from a single device. This module eliminates network downtime due to single points of fault, resulting in high reliability and availability for modern digital substation applications as mandated by the IEC 61850 standard.
- Partnership brings together leading-edge integrated circuit (IC) methodologies, processes and tools to help the automotive supply chain solve design and verification challenges
- Leveraging Arm automotive IP and software within Siemens’ PAVE360 digital twin environment enables collaboration and empowers automakers and suppliers to develop and validate differentiated safety enabled systems, ICs and software solutions in the context of the entire vehicle
- Siemens’ PAVE360, part of Siemens Digital Industries Software’s Xcelerator portfolio, helps automotive companies innovate and develop the complex electronic systems needed for today and tomorrow’s vehicles
Siemens Digital Industries Software today announced a partnership with global semiconductor IP leader Arm, that will bring leading edge IP, methodologies, processes and tools together to help automakers, integrators and suppliers collaborate, design and bring to market their next-generation platforms much faster. This partnership was formed to address the increasingly complex challenges facing the industry in developing platforms to realize active-safety, advanced driver assistance, in-vehicle infotainment, digital cockpits, vehicle-to-vehicle/vehicle-to-infrastructure and self-driving vehicles. Key advances in computing and sensor technology are enabling companies to redefine mobility beginning with the integrated circuits and software within automotive electronics systems. The combination of Siemens’ and Arm’s innovative technologies can help automakers and suppliers deliver tomorrow’s electronic design and automotive solutions, today.
- Voltage variant of Sinamics G120X for USA and Latin America
- Save space with new size for the Sinamics V20
- Adapter kit to physically and thermally separate power module and control unit for Sinamics G120
With numerous innovations, Siemens is extending its drive portfolio, improving user-friendliness and offering space-saving installation options. The Sinamics G120X converter, designed specifically for use in water/wastewater applications and in HVAC systems, is now also available in a three-phase 3AC 200V voltage variant in the power range up to 55 kW. This means that the converters can now be integrated seamlessly into applications in the USA and in Latin America. Due to its robust construction and the coating of the PCBs according to 3C3 standard the converter is suitable for harsh environments. The new module for extending the digital and analog inputs and outputs increases the flexibility and the optimal control of converter-guided applications. The Sinamics G120X now also supports the communication protocols Profibus, Modbus RTU, USS and BACnet MS/TP. It is equipped with extensive interfaces and can be easily integrated into existing or new systems.
- New power output module boosts HCS4300 heating control system performance
- HCS4200: space-saving solution for use in flat control cabinets with new CIM4210C central interface module
- Simple, convenient engineering and commissioning of industrial heating processes with TIA Portal
Siemens
has equipped the modular Siplus HCS heating control systems for
switching and controlling heater fields and elements with a new power output
module (POM) and a central interface module (CIM). With more power per output
and a space-saving solution for mounting in flat control cabinets, the flexible
heating control system is now even more versatile, and can be used for example
in applications with heat registers.