- U5 and U8 metro lines to receive modern
Trainguard MT train control system for semi-automated (GoA2) operation
- With CBTC, headways can be shortened, and line capacity increased
by up to 30%; conversion to be completed by 2032 during ongoing operations
Siemens
Mobility has won the tender from Berliner Verkehrsbetriebe [BVG] and will
introduce a Communications-Based Train Control System [CBTC] on the U5 and U8
metro lines in Berlin for the first time. The state-of-the-art Trainguard MT CBTC
solution will enable semi-automated operation (GoA2: Grade of Automation) on
the U5 line by 2029 and on the U8 line by 2032, increasing capacity on these
lines by around 30%. Technically speaking, CBTC technology even allows headways
of less than 100 seconds. This technological advance will also significantly
improve the reliability and punctuality of the two metro lines. Siemens
Mobility will carry out the conversion during ongoing operations so that trains
on both lines of Germany’s largest metro system can continue to run
uninterrupted throughout the entire project. The contract has a volume of
approximately 200 million euros, plus additional long-term technology
maintenance contracts.
- First cross-country project in the Middle East and Arab World connecting
the Emirati capital Abu Dhabi in the United Arab Emirates to Sohar in the
Sultanate of Oman; length of 303km
- The Oman section of the network marks the first railway system to be
delivered in history of the Sultanate of Oman
Siemens Mobility, together with its consortium partner Hassan Allam Construction, is
honored to announce that it has been awarded the Abu Dhabi – Sohar Design and
Build Railway Systems and Integration contract by Oman – Etihad Rail, a joint
venture co-owned by the two countries to deliver this network. Siemens Mobility and
Hassan Allam Construction will deliver the design, build and integration of the ETCS
Level 2 signaling, telecom and power supply systems over the 303-kilometer-long
Abu Dhabi – Sohar railway link. The signaling solutions are state-of-the art and
desert-proof. This project marks the first-ever cross-country railway network in the
Middle East and Arab world.
- Communications-based Train Control
(CBTC) Signaling system and Platform Screen Doors (PSD) to be provided on for
Cross Island Line in Singapore
- The intelligent infrastructure will
provide greater availability, enhanced operations, and will improve passenger
experience
Siemens Mobility has been awarded a contract
by the Singapore Land Transport Authority (LTA) to provide a signaling system
(CBTC) and full-height platform screen doors (PSD) for the Cross Island Line
(CRL). The order is worth approximately €310 million.
- East Rail Line Cross-Harbour Extension equipped with new signaling system officially opens for revenue service
- 46 km East Rail Line now connects Chinese Mainland border, New Territories, Kowloon to Central Business Districts on Hong Kong Island
- Automatic train control system on the whole East Rail Line enhances operational efficiency
The East Rail Line Cross-Harbour Extension in Hong Kong successfully commenced passenger service on May 15, 2022, with Siemens Mobility’s Communications-Based Train Control system (CBTC). This completes the automation of the 46 km long East Rail Line connecting the Chinese Mainland border to the central business areas on Hong Kong Island and becomes the fourth railway line crossing Victoria Harbour. The Siemens Mobility digitalized signaling system helps provide passengers with the ability to reach the commercial, convention and financial hubs in the Wan Chai North and Admiralty areas in a faster, safer, and more seamless way.
- Hamburger
Hochbahn and Siemens Mobility are building the train control system of tomorrow
for Hamburg’s U2 and U4 lines
- Significant
increase in capacity: trains will be able to run at 100-second intervals
Between now and 2030, a state-of-the-art digital train
control system from Siemens Mobility will be installed as an upgrade to the
conventional train control system used by operator Hamburger Hochbahn
(HOCHBAHN) on its U2 and U4 subway lines. The new technology, known as CBTC
(communication-based train control), will allow trains to run at shorter
intervals of only 100 seconds, which will put significantly more trains on the
track in the future, thereby increasing capacity. In addition, CBTC also
improves punctuality, reliability, and energy consumption.
- Expansion of existing partnership with transit
operator Metrolinx
- Increasing system availability and reliability for
Toronto’s passenger railway system
Siemens
Mobility has been chosen by Metrolinx, the regional public transit operator
for the Greater Toronto and Hamilton Area, to handle their track, signal, and right-of-way maintenance for the
Central Region of Toronto's passenger railway infrastructure system. This
partnership builds upon Siemens Mobility's existing maintenance services in the
West Region and signal and communications services at the Metrolinx Network
Operations Center.
- Latin America’s first fully automated metro line (GoA 4)
- Siemens Mobility digitalized CBTC technology installed across entire 15 km of track,11 stations, and 29 trains
- Automated signaling provides greater availability, enhanced operations, and passenger experience
ViaQuatro has successfully begun full operation of São Paulo’s entire Metro Line 4 with Siemens Mobility’s Communications-Based Train Control (CBTC) signaling. Since its first stretch opened in 2010, it has been the first fully automated metro line in South America that can operate with GoA 4, the highest grade of automation that allows trains to be automatically controlled and operated. The digitalized and optimized system allows for a more efficient and centralized control of operations, while also increasing the safety, availability, and capacity across the entire network.
- CBTC to be
installed on the Johor Bahru-Singapore Rapid
Transit System
- First case
where CBTC technology is used on a cross border link
- Rail line will
ease current congestion, improve cross-border connectivity, and bolster
economic activity in the region.
Siemens
Mobility has been awarded a contract by RTS Operations to design, install and
commission a Communications-Based Train Control (CBTC) signaling system and
Platform Screen Door System on the Johor Bahru-Singapore Rapid Transit (RTS)
Link. This will be the first ever case of CBTC technology being used on a cross
border rail link. The 4 km system connecting Johor Bahru, Malaysia and
Woodlands, Singapore will be operated by RTS Operations, a joint venture between
Singapore rail operator SMRT and Malaysian public transport firm Prasarana.
Once completed, the RTS Link will be able to transport an estimated 10,000 passengers an
hour in each direction, helping ease current congestion at existing border
entry points, improving cross-border connectivity and bolstering economic
activity in the region. The line will also be equipped with GoA 4, the highest grade
of automation that allows for trains to be automatically controlled and
operated.
- HMH,
s.r.o is the manufacturer of the MIREL, a train protection system for Slovakia,
Czech Republic, Hungary, and Poland
- Acquisition
strengthens Siemens Mobility's position as a leading rail infrastructure provider in Europe
Siemens Mobility has completed the
acquisition of HMH, s.r.o., a Slovakian-based technology company, that offers
the MIREL national train protection system for Slovakia, Czech Republic, Hungary,
and Poland. With this acquisition, Siemens
Mobility is now able to offer a complete train protection portfolio covering
the Eastern European rail corridors. HMH will remain based in Bratislava,
Slovakia, and will be integrated into Siemens Mobility’s Rail Infrastructure
business unit.
- More space for locomotive production and service business
- Floor area to be increased by around 30,000 m2
- New capacities to meet growing demand
Siemens
Mobility is expanding its manufacturing and services facility in Munich-Allach
in order to meet the growing demand for locomotives and services. The factory
will be enlarged to 80,000 m2 from its current 50,000 m2
to provide additional capacities for processing new orders, optimizing
production and logistics flows within the facility, and add more office space.