Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release18 May 2022Siemens Mobility GmbHMunich
Hong Kong’s East Rail Line extension opens with Siemens Mobility CBTC technology

“The opening of the East Rail Line Cross-Harbour Extension is a significant milestone for public transportation in Hong Kong, which provides the people of Hong Kong with a fourth cross-harbour rail connection. Our state-of-the-art signaling solutions will increase the reliability, availability, and efficiency of the entire 46 km and 16 station East Rail Line,” said Andre Rodenbeck, CEO of Rail Infrastructure at Siemens Mobility. “We have successfully implemented more than 40 CBTC systems across the world. This important project further underscores our leading position in the field of urban mobility.”
Siemens Mobility equipped CBTC at 16 stations on the East Rail Line, while also modernizing and expanding the railway network by 6 km and three additional stations. The radio-based technology enables real-time data to be captured on vehicle position and speed conditions. This allows the East Rail Line to safely accommodate an increased number of vehicles on the line at a greater frequency. Additionally, the upgraded digitalized system provides the ability to continuously receive updates on system status which improves operational efficiency, resulting in fewer delays and more up-to-date travel information.
Along the East Rail Line and its Cross-Harbour Extension, the Siemens Mobility solution Airlink has been installed for radio transmission, and automatic train supervision is realized through the operations control system. Electronic interlockings and Trainguard MT (TGMT) Wayside Control Units have been installed for efficient train control. Eventually, a total of 37 passenger trains and 22 locomotives will be equipped with Siemens TGMT On-Board Computer Units (OBCU). The new system is controlled and monitored by the Operations Control Center in Tsing Yi.
The Siemens Mobility CBTC solution Trainguard MT is the most extensively deployed automatic train control system in the world and is used by many operators, including Paris, Beijing, New York, London, and Copenhagen.
Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2021, which ended on September 30, 2021, Siemens Mobility posted revenue of €9.2 billion and had around 39,500 employees worldwide. Further information is available at:
www.siemens.com/mobility.
Reference Number: HQMOPR202205176460EN