- SICAM 8 delivers a universal automation platform for all applications in the field of power supply
- Incorporates SICAM HMI, elevating process visualization to the next level
- Includes the SICAM S8000 software solution for power automation
- SICAM 8 platform forms part of the Siemens Xcelerator portfolio
Siemens Smart
Infrastructure has launched the highly scalable SICAM 8 power automation
platform. Designed with scalability and security at its core, the platform helps
customers achieve resilient and secure grid operation, while allowing for the
incorporation of additional applications in the future. It also includes two
new software solutions: the SICAM HMI (Human Machine Interface) visualization
tool and the SICAM S8000 software solution for power automation, and forms part
of the Siemens Xcelerator portfolio, an open digital platform that enables
customers to accelerate their digital transformation easier, faster, and at
scale.
- Prototype Megawatt Charging System [MCS] from Siemens successfully delivered a 1MW charge
- The new technology highlights the potential for megawatt charging to redefine long haul trucking
- The Siemens SICHARGE Megawatt Charging System used is based on its SICHARGE portfolio with a customized MCS dispenser
Siemens Smart Infrastructure has completed the first successful 1MW charge, in a pilot which brought together a prototype MCS charging station from Siemens and a long-haul prototype eTruck from a well-established OEM.
- Bustanica, the Dubai-based vertical farming company, requires 95% less water than a conventional plot, and yields more than 1 million kg of produce free of pesticides, herbicides and chemicals
- Siemens provided building systems and automation hardware and software from its Digital Industries and Smart Infrastructure portfolios
- Building systems, automation software and hardware are part of Siemens Xcelerator
Siemens provided automation and building technology
to the recently opened Bustanica vertical farm in Dubai, the world’s largest of
its kind. The $40 million facility is owned by Emirates Crop One, a joint venture
between Emirates Flight Catering, one of the world’s largest catering
operations serving more than 100 airlines, and Crop One Holdings Inc., an
industry leader in technology-driven indoor vertical farming.
- Support reliable power supply for 965,000 citizens in Stockholm area
Ellevio, Sweden’s second largest grid company, has contracted Siemens Smart Infrastructure to deliver a new grid control system for its distribution network. The new grid control system based on Spectrum Power 7 will improve handling of increased network complexities, abnormalities, and security threats, whilst enabling improved ease and use for operators. Ellevio's control center in Karlstad is responsible for providing a reliable energy supply for 965,000 citizens in Sweden. The grid control is set up in a flexible multi-site operation with a main control center in Karlstad and a supporting control center in Stockholm for back-up.
- 2-loop fire control panel connects up to 252 devices
- EN 54-23 compliant alarm devices and dedicated peripherals
- Time-saving tools such as auto configuration and on-board web server
- License free programming
With the launch of the new version of the fire protection system, Cerberus FIT, Siemens Smart Infrastructure expands its offering for the small to medium-sized buildings market. Various small to medium-sized buildings can now be covered with a simple and cost-efficient solution. Cerberus FIT maximizes fire safety, thanks to greater functionality and enhanced productivity for those working on protecting the buildings. The intuitive interface as well as the auto configuration tool allow the technician to install, commission and maintain the system in a fast, easy and reliable way. With the delayed alarm function staff will be informed first to identify what an alarm is about in order to assess the situation. This ensures business continuity and reduces disturbances to occupants of smaller buildings such as small-to-medium sized hotels, kindergartens or nursing homes.
- Continuous monitoring of energy consumption in the terminal building and at the shore power connecting points
- IoT data platform enables data storage in MindSphere and easy remote access
- Systematic energy data management ensures efficient operations
The Port of Kiel commissioned Siemens Smart Infrastructure to implement a cloud-based power monitoring solution for its shore power system. The shore power system, also from Siemens, will cover the electricity demand of all ships at the Ostseekai and Schwedenkai with green power while they are berthed at the Port of Kiel. This saves more than 8,000 tons of CO2 per year. The new power monitoring solution makes it possible to measure the energy consumption in the shore power operations building and at the Ostseekai and Schwedenkai connecting points, and store the data in MindSphere, the cloud-based IoT system from Siemens. The operators have access to all relevant electrical values at any time and from anywhere, allowing them to determine consumption, identify faults, avoid downtimes, and plan maintenance routines better.
- Reliable protection with minimal space requirements
- For power distribution and industrial plants
Siemens Smart Infrastructure presents the new Siprotec 5 Compact device, specially designed to address the demands of industrial applications, infrastructure and distribution grids. With its compact size, large number of inputs and outputs, and universal range of functions, it can be configured to meet the specific requirements associated with protecting feeders and motors. As a space-saving universal device, it is ideally suited to help optimize investment and operating costs in power distribution.
- New Grid Diagnostic Suite offers unique comprehensive insights
- Gain a grid-wide view of energy automation systems
- Market launch of initially four cloud-enabled applications
- Enhances cost efficiency and availability of smart grids
- Support through digitalization in increasingly complex power grids
Siemens is presenting for the first time its new Grid Diagnostic Suite at the European Utility Week in Paris. The Grid Diagnostic Suite initially includes four cloud-based applications which collect data from new or existing field devices for protection, distribution automation and power quality. These data are stored and analyzed in the cloud. This requires almost no additional engineering effort. Distribution grid operators and operators of electricity grids in industrial parks can quickly tap into useful information from devices installed anywhere in the smart grid. This will enable grid faults, for example, to be detected at an early stage and quickly rectified. After information is collected, vulnerabilities can be identified, and necessary measures can be implemented before any damage occurs. In this way, Internet of Things (IoT) applications in the Grid Diagnostic Suite enhance the availability of power grids while enabling them to be operated cost-efficiently.
- System based on Siemens Spectrum Power supports second-by-second control of all assets and integration of RWE wind and solar farms
- Improved combination of electricity generation from renewables and conventional fuel is a major milestone for the energy transition
RWE is making its power station control system fit for the future by adopting a new technology. Optime, a new SCADA system based on Siemens Spectrum Power, gives RWE a uniform control technology. SCADA stands for 'Supervisory Control and Data Acquisition' – in other words monitoring and managing technical processes using a computer system. Previously, there were two separate systems: one for power plants in Germany and another for the Netherlands and Belgium. The new solution combines the two, while integrating RWE’s renewable energy assets in Europe. It can also accommodate additional units such as battery storage systems and diesel-powered backup generators.
- Portfolio serving entire power range from 50 to 600 kW
- Flexible combination with connection options as cable and pantographs
- For fast and secure charging at the depot and en route
- Cloud-based control and monitoring of charging processes
At Busworld 2019, Siemens is presenting its Sicharge UC family for charging electric buses, trucks and duty vehicles at the depot and en route. The Sicharge UC charging system covers the entire power range from 50 to 600 kilowatts (kW) and can be combined with several connection options such as charging plugs and offboard or onboard pantographs. To meet growing demands from the vehicle industry for higher voltages, the station can operate at up to 1,000 volts (V). Electric vehicles with various technologies and batteries can therefore be charged flexibly, either en route or at the depot. The charging processes can be monitored and controlled via a MindSphere application. MindSphere is the cloud-based, open IoT operating system from Siemens.