Labeled as the project of the century for the German metropolitan region, the Rhine-Ruhr express (RRX) will help alleviate the continuously worsening transportation issues along the Rhine and Ruhr from 2018. The municipalities involved in the new RRX rail transport concept commissioned Siemens to supply 82 electric multiple units, type Desiro HC, and to provide maintenance services for a period of 32 years. With a total volume of more than 1.7 billion euros, this is the largest regional rail service order in Germany so far for Siemens.The region is one of the largest conurbations in Europe, with a population of approximately ten million and numerous transit routes. On the main section between Cologne and Dortmund in particular, mobility has been heavily restricted for years now by overstretched public transport networks and train connections. Through a targeted extension of the railway network and the shift of traffic from road to rail this enables, the RRX is expected to replace roughly 31,000 individual car trips every working day. The first RRX trains will begin operating punctually with the change of the rail system's timetable on December 9, 2018. Commercial operation will begin on Line RE 11 that connects Düsseldorf, Essen, Dortmund, Hamm, Paderborn and Kassel. During rush hours the eventual target is one train every 15 minutes.
Bane NOR, the state-owned agency responsible for the Norwegian national railway infrastructure, has contracted Siemens to upgrade the signaling equipment of the entire Norwegian rail network to the European Train Control System (ETCS). Commissioning of the rollout lines is scheduled to be completed by 2034. The contract also includes services for 25 years and is worth around 800 million euros in total.
Siemens Mobility, Inc., a fully owned subsidiary of Siemens AG, is a leading international provider of intelligent mobility solutions that offer guaranteed availability, optimized capacity and enhanced passenger experience. The company’s business includes rail rolling stock, rail automation, intelligent traffic systems, traffic telematics systems as well as rail electrification. The portfolio also covers turnkey mobility projects and tailored financing solutions.Siemens Mobility, Inc. draws on more than 160 years of expertise and experience in transportation. The company combines innovations with comprehensive industry know-how, a global network of recognized experts in over 40 countries, and the solid financial base of Siemens AG.
South-west Germany is counting on Siemens: from 2020 onward, DB Regio AG will be operating its Rhine Valley rail network exclusively with new trains from Siemens. The German Railways order covers 15 Desiro HC and 24 Mireo trains in total, and goes hand in hand with a restructuring of the rail transport services in the Rhine Valley. There is a clear separation between a rapid train system for fast cross-regional services and a regional suburban rail system (S-Bahn) with stops at all stations. The Mireo will be deployed as a regional train (RB) service along the line section from Offenburg via Freiburg to Basel/Neuenburg (Switzerland) as well as in the Kaiserstuhl area on Sundays between Freiburg and Endingen/Breisach. The line section from Karlsruhe via Offenburg and Freiburg to Basel (Switzerland) will be operated with the Desiro HC as a regional express service.
Connected and self-driving vehicles are on the horizon. Autonomous taxis and minibuses could cover the last mile between homes and public mass transit and long-distance transport hubs, helping make private cars superfluous in cities and relieving congestion. In rail transport as well, fully automated systems and connectivity can help satisfy the rapidly growing demand for mobility. Making vehicles and infrastructure more intelligent can ensure better availability and make mobility safer. All this adds up to vastly improved urban environments.Siemens is working with municipalities, public transit authorities and research institutes to develop these transport concepts.
On March 2nd, 2017, German Chancellor Angela Merkel, Egyptian President Abdel Fattah El-Sisi, Siemens CEO Joe Kaeser and further high-ranking representatives witnessed the symbolic inauguration of the first phase of Siemens' megaproject in Egypt. The event marked an important milestone towards the completion of the project.In collaboration with the Egyptian Ministry of Electricity and Renewable Energy, Siemens and its consortium partners, Orascom Construction and Elsewedy Electric, announced on July 24, 2018 the completion of the Egypt Megaproject in record time. The parties celebrated the combined cycle commissioning and the start of operations at the Beni Suef, Burullus and New Capital power plants. The stations will add a total of 14.4 gigawatts (GW) of power generation capacity to Egypt's national grid, enough power to supply up to 40 million people with reliable electricity. With this milestone, Egypt and Siemens have set a new world record for execution of modern, fast-track power projects, delivering 14.4 GW of power in only 27.5 months. A single combined cycle power plant block with a capacity of 1,200 megawatts typically takes approximately 30 months for construction. For the Egypt Megaproject Siemens in parallel built twelve of these blocks in record time and connected them to the grid.Following the delivery of several Siemens SGT5-8000H gas turbines, the first steam turbine for the Egypt Megaproject began its journey in December 2016 from the Siemens factory in Muelheim to the power plant Beni Suef in Egypt. The main components of the 670-ton cargo were lifted with a heavy-duty crane from the production hall onto a transport vessel standing by at the plant's inland harbor facilities. The vessel transported the SST-5000 steam turbine from Muelheim to the deep-water port of Antwerp where it was loaded onto a heavy cargo ship and transported to Egypt.After the steam turbines installation, the waste heat from the gas turbines will be used to produce steam that will then drive the steam turbine, thus increasing the overall power output and efficiency of the power plant. In total, Siemens will deliver twelve SST-5000 steam turbines for the Egyptian power plants Beni Suef, Burullus and New Capital. All of these steam turbines will be manufactured at the Siemens factory in Muelheim.
Austrian Federal Railways (ÖBB) has ordered a total of 189 Desiro ML regional trains from Siemens. The trains will operate under the name "Cityjet".The trains will be produced at the Siemens Mobility plants in Krefeld, Germany, and Graz, Austria, and final assembly will take place at ÖBB's Technical Services factory in Jedlersdorf, Austria.Two design alternatives of the Desiro ML are built: the urban train design for large metropolitan areas such as Vienna and the regional train design. The ÖBB cityjet also offers a variable, low-floor seating arrangement as well as spacious entrance and intercar gangway areas, an attractive, innovative design and maximum riding comfort, and barrier-free entrance to all 550-mm station platforms in Austria.Austrian Federal Railways (ÖBB) and Siemens Mobility are jointly investing in the future of passenger transport and are developing an electro-hybrid battery drive for trains. Operating as a battery-powered train, the Cityjet eco is an alternative for non-electrified rail lines primarily served at present with diesel-powered passenger trains. Battery operation can reduce CO2emissions by up to 50 percent compared to diesels. Following extensive testing of the prototype train, it is expected to first be used in passenger service in the second half of 2019.On August 26, the joint project reached its next milestone: The battery driven EMU got the homologation and is starting passenger service beginning of September 2019, bringing more sustainability to non-electrified tracks in Austria.