- Early detection of anomalies in the drivetrain with the support of artificial intelligence
- Trend Prediction for optimized maintenance efficiency
- Higher productivity and reduced machine and system downtime
Siemens has supplemented the Mindsphere application Predictive Service Assistance with an AI-based module. The new Artificial Intelligence module identifies concrete fault patterns in motors at an early stage, such as misalignment or a defective bearing. The application thus helps users to reduce downtimes and further improve spare parts and maintenance processes. The new Artificial Intelligence module for motors uses a neural network to solve what was previously implemented using a defined KPI limit value. This enables the module to detect anomalies even before the defined limit value and provides clear indications of the type and severity of faults and their development. As soon as the application detects signs of an error, it warns the user and generates a due date that indicates when the error should ideally be corrected and what corrective action is recommended to prevent an unplanned downtime. Predictive Service Assistance with the new AI-based Artificial Intelligence module is offered as part of a Predictive Service Assessment. The package includes a customized configuration service that ensures that the Mindsphere application with the new AI-based module runs optimally according to the customer's requirements.
- Industrial Edge V1.0 comprising the Edge Management system, edge apps, and edge devices with container-based runtime
- Edge Management system provides central management for edge devices and apps over the entire lifecycle
- Apps that increase productivity can be integrated into industrial environments quickly, with little effort and minimal risk
Siemens is
expanding its offer for industrial IoT solutions, adding to its Industrial Edge
portfolio a central and company-wide scalable infrastructure for managing
connected edge devices and apps. With the new Industrial Edge Management
system, users can remotely monitor the status of every connected device and
remotely install edge apps and software functions on distributed edge devices.
In combination with existing hardware and software products, this Industrial
Edge V1.0 open platform provides users with a ready-to-use and seamless
solution for data processing on the production level with integrated device and
app lifecycle management.
- Research projects with volume of €1.7 million and term of 30 months
- Studies of highest automation levels in regional and mainline transport
- Important impetus for digitizing railways
Siemens Mobility and prominent partners have won two innovative research projects from the German Center for Rail Traffic Research (DZSF) to study the safety of automated rail operations. The aim is to define the criteria needed for approving fully automated regional and mainline rail service. The two projects will be funded with €1.7 million and are scheduled to run for 30 months.
- High-frequency data exchange between Sinamics drives and the Industrial Edge platform
- Drive System Framework for connectivity, management, and configuration of the Digital Twin
- Paving the way for new business models
As part of
the Digital Enterprise SPS Dialog, Siemens is launching Analyze MyDrives Edge,
its first edge application for drives. The company is thus demonstrating in
concrete terms how edge computing can make Sinamics drive systems even more
intelligent and what benefits users and machine builders can derive from it.
Analyze MyDrives Edge is being launched with basic functionalities similar to
the proven Mindsphere application Analyze MyDrives but will be enhanced with
intelligent features based on high-frequency data exchange. The Edge
application thus allows users of machines and industry applications to perform
complex analyses of data that is already collected in the drive. Machine
learning and AI algorithms on which the edge application is based identify
patterns and detect anomalies and their causes, thus providing timely
indications of any pending machine maintenance. This minimizes downtimes and
reduces the consumption of resources.
- Siemens presents liquid-cooled, robust power conversion system based on proven Sinamics S120 platform
- Grid converter comes with certification in accordance to VDE-AR-N 4110 and with validated simulation model for easy project planning, optimization and integration into the power grid
With Sinamics PCS, Siemens presents a new power conversion system for battery storage applications. The Sinamics PCS grid converter makes locally generated battery power usable for industrial and public power grids. Sinamics PCS controls the charging and discharging process of the battery and helps to handle load peaks and grid disturbances via the battery storage, to store the electricity in an energy- and cost-efficient manner and to bring the energy stored in batteries efficiently and reliably into the grid.
- Growing demand for remote access via public 5G networks for remote maintenance
- Scalance MUM856-1 connects local industrial applications to the public 5G network
- Sinema Remote Connect management platform provides secure access to remote plants and machines
Siemens presents the first industrial 5G router for connecting local industrial applications to a public 5G network. The device will be available in spring 2021. Using the newly developed Scalance MUM856-1, industrial applications such as machines, control elements, and other devices can be accessed remotely via a public 5G network, providing a simple remote maintenance option for these applications using the high data rates offered by 5G. The Sinema Remote Connect management platform for VPN connections can be used to provide easy and secure access to these remote plants or machines – even if they are integrated in other networks.
- Simatic Robot Integrator with Simatic Robot Library makes engineering easy for robots in the TIA Portal
- Universal interface supports integration by all robot manufacturers
- Re-usable program codes thanks to standard programming language
- Time savings of up to 30 percent for engineering
Siemens presents the Simatic Robot Library for the Simatic Robot
Integrator - a new universal robot library for the TIA (Totally Integrated
Automation) Portal, which replaces the previous manufacturer-specific
libraries. The specification has been developed in close cooperation with robot
manufacturers ABB Robotics, Comau, Epson, FANUC, Kawasaki Robotics, KUKA,
Panasonic Industry, STÄUBLI, Techman Robot, Yamaha, and YASKAWA. In future,
users will be able to program most of the robots available on the market in the
TIA Portal using the Simatic Robot Library, and make use of standard operating
concepts based on the Simatic Robot Integrator and Simatic HMI.
- Siemens Mobility supplying the complete system technology for C-ITS in Austria
- C-ITS allows for exchange of information between vehicles and the road via ITS-G5 broadcast technology
- ASFiNAG is the first infrastructure provider in Europe to install C-ITS
Siemens Mobility is pleased to announce that it is
partnering with ASFiNAG, the operating authority for the Austrian highway network,
to provide the technology for an intelligent traffic
management system that facilitates the exchange of safety information between
vehicles and the road. The “Cooperative Intelligent Transport System”
(C-ITS) is a next generation traffic management system that uses
broadcast technology to analyze roadway conditions and disseminates information
to motorists relating to traffic jams, accidents, and lane
closures. ASFiNAG is the first infrastructure
provider in Europe to reach the milestone of installing a network connecting
the vehicle and road. The process of implementing the system across 2,200
kilometers of highway and expressway in Austria has already started.
- “Digital Enterprise SPS Dialog” virtual event on November 26, 2020: participants can discover highlights in 3D and join the dialog with Siemens experts
- New products, services, and solutions for the Digital Enterprise portfolio ensure more flexible production for rapidly changing requirements
- Numerous practical exhibits and models visualize digital progress along the entire value chain
Around SPS Connect, Siemens is hosting a
special virtual event to present new products, services, and solutions for the
Digital Enterprise portfolio,
which companies in the manufacturing and process industry can use to react to
rapidly changing market requirements and conditions. Siemens brings more
intelligence and therefore greater flexibility to production – taking industry
to the next level. This
is achieved by combining automation and digitalization solutions with cutting-edge
technologies such as artificial intelligence, edge and cloud computing or
additive manufacturing. Using
this link https://sie.ag/2TIM1AO, interested
parties can register for the “Digital Enterprise SPS Dialog” virtual event on
November 26, 2020, enabling them to discover the topics in a virtual 3D
showroom and join the dialog to extend their knowledge.
New products include a ready-to-use open
Industrial Edge platform, new edge hardware, and a new edge application for
drives. A new distributed
drive system is also being launched. Further innovations this year include a solution for
multi-vendor programming of robots in the TIA (Totally Integrated Automation)
Portal, innovative Cloud Connect products for integrated data access, and new Connectivity
and Remote Collaboration Services.
- Flexible capacity expansion thanks to quick availability
- Reliable operation with sophisticated technology
- Attractive price based on standardization
Siemens Mobility is presenting the new Mireo Smart train today. It enables operators to quickly expand their capacity and ensures profitable operation thanks to its attractive price, low maintenance costs and very high degree of reliability.