-
Series
483/484 now running on S47
-
Ten
pre-series trains begin service in January
-
More
comfort and space for passengers
The New Year is starting off with a premiere! Shortly after midnight on
January 1, the first train of the new series 483/484 S-Bahn will start
passenger service in Berlin.
- The new series 483/484 trains are waiting to begin service – Premiere run on New Year’s Eve on line S47
The countdown for a new S-Bahn era has begun! Two weeks before their inaugural run on January 1, the new series 483/484 trains are ready and waiting to be deployed.
- On-time handover of 84
th and final train for the Rhine-Ruhr Express
(RRX)
- The RRX train offers highly innovative, digitally networked, and
high-performance mobility service for people in the Rhine-Ruhr region
- Digital maintenance ensures nearly 100-percent availability
The 84
th
train for the Rhine-Ruhr Express (RRX) infrastructure and mobility project was handed
over right on schedule. The trains were originally ordered from Siemens
Mobility in 2015. The RRX order, consisting of trains and a service contract,
has a total volume of €1.7 billion and marks the largest order received by
Siemens Mobility to date in the sector of regional rail passenger transport in
Germany.
- One single device for lines of up to 500 km
- Monitoring for powered, unpowered or grounded lines
- Highly precise localization of line faults
- Simplifies maintenance and increases network reliability
Siemens Smart Infrastructure recently launched its new PowerLink CM, a condition monitoring solution for high-voltage AC and DC transmission lines. To ensure reliable power supply, optimize grid utilization and prevent blackouts the device is designed to precisely locate faults in the transmission grid and continuously track line conditions. One single PowerLink CM device is sufficient to monitor line lengths of up to 500 km. Faults as well as line condition can be detected in powered, unpowered or grounded lines. Fault reports are received by the affected substation and are forwarded from there to the control room. For continuous line monitoring, the device can be connected to MindSphere, the open cloud-based Internet of Things (IoT) platform from Siemens, which facilitates transparent processing of all line data in the cloud. This allows grid operators to analyze status reports and optimize maintenance activities.
- Charging, medium and low-voltage technology for two carports at Hamburger Hochbahn AG’s Alsterdorf bus depot
- Space-saving installation as technical center on carport’s roof
- Important step for transitioning to climate-friendly local transport in Hamburg
Siemens Smart Infrastructure won a major contract from Hamburger Hochbahn, the largest local transport provider in the Hanseatic city. Siemens will equip two of the six carports at the Alsterdorf bus depot with a total of 96 charging points as well as medium and low-voltage technology. Operations are scheduled to start in summer 2021. With a total of 240 parking spaces, it is one of the largest and most modern bus depots for electric buses in Europe.
- First CBTC project in India with GoA 4, the highest grade of automation
- Will allow for trains to be automatically controlled and operated
- Automated signaling and train operations will provide greater availability and enhance operations and passenger experience
Siemens Mobility and Siemens Limited India is partnering with Bengaluru Metro Rail Corporation Limited (BMRCL) to implement a comprehensive set of automated train solutions for phase 2 of the Bengaluru metro expansion project. This will be the first CBTC project in India with GoA 4, the highest grade of automation that allows for trains to be automatically controlled and operated. Siemens Mobility will install its communications-based train control (CBTC) system across 18.8 km of the Yellow Line, which will feature electronic interlockings, an automatic train protection and supervision system, as well as a telecommunication system. The automated signaling and train operations will allow BMRCL to run trains 90 seconds apart, providing greater availability and an enhanced passenger experience.
- FIA and Siemens extend partnership to provide the ‘FIA Mobility Advocate’— a unique software and hardware toolkit — for FIA Mobility Member Clubs to strengthen advocacy of future transport solutions
As an
“Official Supplier of Urban Mobility Advocacy Solutions” for the Fédération Internationale de l’Automobile (FIA), the governing body of world motor sport and
the federation of the world's leading motoring organisations, Siemens plans to
develop a toolkit of software solutions for FIA Member Clubs to help them
provide an evidence-based approach to advocate for the implementation of mobility
policies and strategies. The ‘FIA Mobility Advocate’ combines modeling for
mobility, autonomous vehicles, and the environment, with enhanced analysis
outputs to help meet current future mobility goals.
- Siemens and Hassan Allam Construction to build new control center located in Egypt’s New Administrative Capital
- Customer is Egyptian Electricity Transmission Company
- Latest software to monitor, manage and control extra-high voltage transmission networks and power generation plants across the country
- Contract worth more than EUR 45 Mio.
Egyptian Electricity Transmission Company has awarded a contract to the consortium consisting of Siemens Smart Infrastructure and Hassan Allam Construction to build the new National Energy Control Center in the New Administrative Capital of Egypt. The country’s new power grid control center will deploy advanced software and equipment to monitor, manage and control extra-high voltage (220 kV and 500 kV) transmission networks and power generation stations across Egypt. The necessary technologies will be included in the new control center for future grid expansion while maintaining secure energy supply, including intermittent renewable energy sources and storage. The project is expected to be completed by the end of 2022.
- The Mireo train won the Pioneer category of the German Sustainability Award for Design.
The Mireo is the new, eco-friendly and economical regional and commuter train from Siemens Mobility, which offers a comfortable and inspiring riding experience. The first fleet has been in operation since June 2020 in the Rhine Valley in Baden-Württemberg and over 180 trains have already been ordered in the meantime.
- Award honors winners in five categories
- Collaboration with focus on “glocal” value creation, sustainability, and supply chain resilience
- Siemens Mobility’s supplier network helps generate more than 50 percent of revenue
Siemens Mobility announced today the winners of the company’s Supplier Award for 2020. The award honors suppliers who made significant contributions to Siemens Mobility’s success in fiscal 2020 with their outstanding performance. The award was presented in five categories. Trispel GmbH in Germany took top honors in the category “Technology & Innovation.” The category “Logistics Performance” was won by the Spanish firm Industrial de Transformados. India’s Apar Industries was picked best supplier in the category “Competitiveness.” The winner in the category “Quality” was Germany’s ml&s GmbH & Co. KG, and the special “Moving beyond” award went to Lucchini RS in Italy. Over 400 suppliers were invited to the virtual award ceremony. The awards were presented virtually by Karl Blaim, Chief Financial Officer and member of the Siemens Mobility Managing Board, together with Rainer Straub, the company’s Chief Procurement Officer.