- Early detection of anomalies in the drivetrain with the support of artificial intelligence
- Trend Prediction for optimized maintenance efficiency
- Higher productivity and reduced machine and system downtime
Siemens has supplemented the Mindsphere application Predictive Service Assistance with an AI-based module. The new Artificial Intelligence module identifies concrete fault patterns in motors at an early stage, such as misalignment or a defective bearing. The application thus helps users to reduce downtimes and further improve spare parts and maintenance processes. The new Artificial Intelligence module for motors uses a neural network to solve what was previously implemented using a defined KPI limit value. This enables the module to detect anomalies even before the defined limit value and provides clear indications of the type and severity of faults and their development. As soon as the application detects signs of an error, it warns the user and generates a due date that indicates when the error should ideally be corrected and what corrective action is recommended to prevent an unplanned downtime. Predictive Service Assistance with the new AI-based Artificial Intelligence module is offered as part of a Predictive Service Assessment. The package includes a customized configuration service that ensures that the Mindsphere application with the new AI-based module runs optimally according to the customer's requirements.
- Industrial Edge V1.0 comprising the Edge Management system, edge apps, and edge devices with container-based runtime
- Edge Management system provides central management for edge devices and apps over the entire lifecycle
- Apps that increase productivity can be integrated into industrial environments quickly, with little effort and minimal risk
Siemens is
expanding its offer for industrial IoT solutions, adding to its Industrial Edge
portfolio a central and company-wide scalable infrastructure for managing
connected edge devices and apps. With the new Industrial Edge Management
system, users can remotely monitor the status of every connected device and
remotely install edge apps and software functions on distributed edge devices.
In combination with existing hardware and software products, this Industrial
Edge V1.0 open platform provides users with a ready-to-use and seamless
solution for data processing on the production level with integrated device and
app lifecycle management.
- High-frequency data exchange between Sinamics drives and the Industrial Edge platform
- Drive System Framework for connectivity, management, and configuration of the Digital Twin
- Paving the way for new business models
As part of
the Digital Enterprise SPS Dialog, Siemens is launching Analyze MyDrives Edge,
its first edge application for drives. The company is thus demonstrating in
concrete terms how edge computing can make Sinamics drive systems even more
intelligent and what benefits users and machine builders can derive from it.
Analyze MyDrives Edge is being launched with basic functionalities similar to
the proven Mindsphere application Analyze MyDrives but will be enhanced with
intelligent features based on high-frequency data exchange. The Edge
application thus allows users of machines and industry applications to perform
complex analyses of data that is already collected in the drive. Machine
learning and AI algorithms on which the edge application is based identify
patterns and detect anomalies and their causes, thus providing timely
indications of any pending machine maintenance. This minimizes downtimes and
reduces the consumption of resources.
- TIA Selection Tool enables mechanical, electrical and automation planning on a single platform
- Complete standards know-how for electrical planning integrated in one software program
- Time-saving dimensioning of protection and switching devices, including essential design calculations
With “Control Panel Design” Siemens Smart
Infrastructure has integrated new electrical planning features into TIA
Selection Tool, the Siemens configuration and ordering software. This makes
electrical pre-planning completely digital. Now, electrical planners can design
and dimension the main electrical components of a machine quickly, easily, and
in accordance with IEC and UL standards. This reduces the required effort to
perform the task, minimizes potential error sources, and helps machine and
control panel builders improve their competitiveness. TIA Selection Tool is
designed to make it easy and convenient to configure and select all components
of industrial control panels. By integrating the new features, the tool allows
users to design electrical as well as mechanical and automation components
using one set of data and one platform. This lays the foundation for
significantly more efficient development processes, faster lead times, and
smarter electrification solutions for industrial environments.
- Siemens presents liquid-cooled, robust power conversion system based on proven Sinamics S120 platform
- Grid converter comes with certification in accordance to VDE-AR-N 4110 and with validated simulation model for easy project planning, optimization and integration into the power grid
With Sinamics PCS, Siemens presents a new power conversion system for battery storage applications. The Sinamics PCS grid converter makes locally generated battery power usable for industrial and public power grids. Sinamics PCS controls the charging and discharging process of the battery and helps to handle load peaks and grid disturbances via the battery storage, to store the electricity in an energy- and cost-efficient manner and to bring the energy stored in batteries efficiently and reliably into the grid.
- Process bus significantly increases level of digitalization in substations
- Faster installation and commissioning
- Improved system reliability
- Benchmark for future-proof design
Siemens Smart Infrastructure has installed process bus technology at the new high-voltage substation in Los Sauces for one of the largest Peruvian distribution network operators, Luz del Sur. This process bus installation with Siprotec merging units and Siprotec protection devices is one of the first fully digitized energy automation system in operation. The new technology sets benchmarks with its future-proof design and will help optimize the entire operation of the power grid.
- Growing demand for remote access via public 5G networks for remote maintenance
- Scalance MUM856-1 connects local industrial applications to the public 5G network
- Sinema Remote Connect management platform provides secure access to remote plants and machines
Siemens presents the first industrial 5G router for connecting local industrial applications to a public 5G network. The device will be available in spring 2021. Using the newly developed Scalance MUM856-1, industrial applications such as machines, control elements, and other devices can be accessed remotely via a public 5G network, providing a simple remote maintenance option for these applications using the high data rates offered by 5G. The Sinema Remote Connect management platform for VPN connections can be used to provide easy and secure access to these remote plants or machines – even if they are integrated in other networks.
- Simatic Robot Integrator with Simatic Robot Library makes engineering easy for robots in the TIA Portal
- Universal interface supports integration by all robot manufacturers
- Re-usable program codes thanks to standard programming language
- Time savings of up to 30 percent for engineering
Siemens presents the Simatic Robot Library for the Simatic Robot
Integrator - a new universal robot library for the TIA (Totally Integrated
Automation) Portal, which replaces the previous manufacturer-specific
libraries. The specification has been developed in close cooperation with robot
manufacturers ABB Robotics, Comau, Epson, FANUC, Kawasaki Robotics, KUKA,
Panasonic Industry, STÄUBLI, Techman Robot, Yamaha, and YASKAWA. In future,
users will be able to program most of the robots available on the market in the
TIA Portal using the Simatic Robot Library, and make use of standard operating
concepts based on the Simatic Robot Integrator and Simatic HMI.
- “Digital Enterprise SPS Dialog” virtual event on November 26, 2020: participants can discover highlights in 3D and join the dialog with Siemens experts
- New products, services, and solutions for the Digital Enterprise portfolio ensure more flexible production for rapidly changing requirements
- Numerous practical exhibits and models visualize digital progress along the entire value chain
Around SPS Connect, Siemens is hosting a
special virtual event to present new products, services, and solutions for the
Digital Enterprise portfolio,
which companies in the manufacturing and process industry can use to react to
rapidly changing market requirements and conditions. Siemens brings more
intelligence and therefore greater flexibility to production – taking industry
to the next level. This
is achieved by combining automation and digitalization solutions with cutting-edge
technologies such as artificial intelligence, edge and cloud computing or
additive manufacturing. Using
this link https://sie.ag/2TIM1AO, interested
parties can register for the “Digital Enterprise SPS Dialog” virtual event on
November 26, 2020, enabling them to discover the topics in a virtual 3D
showroom and join the dialog to extend their knowledge.
New products include a ready-to-use open
Industrial Edge platform, new edge hardware, and a new edge application for
drives. A new distributed
drive system is also being launched. Further innovations this year include a solution for
multi-vendor programming of robots in the TIA (Totally Integrated Automation)
Portal, innovative Cloud Connect products for integrated data access, and new Connectivity
and Remote Collaboration Services.
- Siemens, MW Storage International, Fluence and Vibeco develop unique ecosystem for global beverage manufacturer
- Solution to enable new levels of energy optimization
- Encompasses software, financing, latest storage technology
- Sinebrychoff’s first energy storage service contract
In a move that brings new market opportunities for industrial players, Siemens has developed a unique business model to support the next level of energy optimization for Finnish brewery Sinebrychoff, a subsidiary of the international Carlsberg Group. At the heart of the solution, which will be implemented at Sinebrychoff’s plant in greater Helsinki, is a virtual power plant (VPP) and the latest energy storage technology, supported with financing solutions, to create one of the first examples of power flexibility in an industrial site.