As part of the pebbles research project,
Siemens, the regional utility Allgäuer Überlandwerk (AÜW) and their project
partners are developing a local electricity market using blockchain technology.
Today, the parties launched pebbles’ electricity trading platform, bringing
them one step closer to creating the first local marketplace for optimized
electricity trading based on blockchain. The platform will be utilized in in
the town of Wildpoldsried in the Bavarian Allgäu region of Germany. Now, during
the platform’s demonstration phase, private producers can use an app to market
their electricity directly to local consumers without going through marketers
or traditional grid operators. The market platform also supports flexible power
from battery storage or controllable loads such as heat pumps or charging
stations for electric vehicles. The blockchain technology, which forms the
basis for managing market transactions, is designed to create end-to-end
transparency and trust between users.
- Siemens and Netze BW cooperating on multi-year field test
- First distribution substation with innovative blue GIS 24 kV ring main unit live in Oberallgäu
- Fluorine gas-free Clean Air switchgear and bio-ester transformer boost sustainability
In conjunction with their ongoing research
cooperation, Siemens Smart Infrastructure and Netze BW GmbH, headquartered in
Stuttgart, have co-developed an intelligent and environmentally-friendly distribution
substation. For the first time, the new station combines the F-gas-free 24
kilovolt (kV) ring main unit (RMU) from the Siemens blue GIS portfolio with a
630 kilovolt-ampere (kVA) distribution grid transformer. Instead of mineral
oil, the Eco Design 2-certified transformer uses fully biodegradable, natural
bio-ester oil for insulation. The integrated automation system from the Siemens’
Sicam portfolio is designed for the special requirements of distributed grids
and enables reliable monitoring and control of the grid. The innovative
substation, which will connect the medium-voltage distribution grid and the
low-voltage local grid in the town of Kreuzthal in the Oberallgäu region, is now
being tested under real-life conditions.
As a virtual event, the Siemens Machine
Tool Days provide insights into digital solutions for the machine tool
industry. Keynotes, #HowTo expert panels and practical examples will deal with
digital possibilities for increasing productivity in manufacturing under the
motto "Digitalization in Machine Tool Manufacturing - Thinking further!
Using the Digital Enterprise portfolio as an example, Siemens will show how the
integration of automation and digitization with future technologies such as
edge and cloud computing and artificial intelligence can be used effectively in
every phase of the value-added chain: from building a digital twin of the
product to production and machine performance to digital services.
> Register here > Explore our agenda
Today, the need for industrial digital solutions is more pressing and more important than ever before. During this event, we want to show how you can benefit from our digital solutions for the machine tool industry - from the Digital Twins of product, production and performance to every aspect of the value chain, including digital services.
- Sinumerik One Dynamics - three technology packages to increase the efficiency of CNC users when programming in the shopfloor and executing CAM-generated CNC programs
- Top Surface and Top Speed Plus for excellent motion control and perfect workpiece surfaces
With the software version NCU-SW 6.14, Siemens is launching three powerful technology packages exclusively for the CNC Sinumerik One. The Sinumerik One Dynamics packages are available in three different packages: One Dynamics Operate, One Dynamics 3-axis milling and One Dynamics 5-axis milling. The software functions contained in the technology packages support users from machine-oriented programming in the jobshop to high-performance machining of CAD-CAM-programmed workpieces with high surface quality.
- Improvement of machine tool availability through predictive maintenance with Analyze MyMachine /Condition
- Analyze MyMachine /Condition for Sinumerik Edge creates a mechanical fingerprint of the machine tool
- Condition evaluation, analysis and comparison of all connected machines using the Mindsphere application
Siemens is extending its edge application Analyze MyMachine /Condition with a corresponding Mindsphere application and thus demonstrating how edge computing and cloud computing can be intelligently combined. The Sinumerik Edge Application Analyze MyMachine /Condition, which the company presented last year at the EMO, uses high-frequency CNC data to create the mechanical fingerprint of a machine tool. In the application, users can capture and evaluate various parameters such as stiffness, friction, and backlash in the individual axes with the help of flexibly configurable measurement series. The measurement results can then be visualized and compared with reference data.
- Adaptable modular solution to deal with short-term needs of hospitals, e.g. during epidemic or temporary construction works
- Ergonomic solution ensuring safety of patients and medical staff
- Compliant with healthcare facilities regulations
- Autonomous care units, fast to deploy, deliver high added value
Siemens Smart Infrastructure has teamed up with Toutenkamion Group to jointly develop an agile container system of highly innovative mobile intensive care units, designed to take pressure off hospital infrastructure. The solution was a response to the Covid-19 pandemic, which forced nursing staff, doctors and hospital managers to urgently come up with practical solutions to ensure adequate care was provided to extremely contagious patients, while maintaining other emergency and conventional care. One of the major challenges of the epidemic has been the need to equip and increase the number of resuscitation and intensive care beds.
- High-frequency radar ensures
reliable readings in challenging environments
- Optional
HMI delivers easy commissioning and diagnostic
support
- Wide
range of liquids and solids applications in practically all market segments
including energy, mining, aggregates and water
Siemens presents two new additions
to the Sitrans LR100 series of 80 GHz radar transmitters. These high-frequency,
compact transmitters deliver robust, reliable measurements even in the most
challenging environments. Both deliver fast and easy setup. Sitrans LR140
features 4-20 mA simplicity and is configured via Bluetooth wireless technology
and the Sitrans mobile IQ App.
- Calibrant Energy to bundle latest distributed energy technologies and financing expertise of global leaders Macquarie and Siemens
- The joint venture will create Energy-as-a-Service solutions from a full range of energy technologies for corporate and municipal clients
Macquarie’s Green Investment Group (GIG), Siemens Smart Infrastructure and Siemens Financial Services (SFS) today announced the formation of Calibrant Energy (Calibrant), a joint venture that offers comprehensive onsite Energy-as-a-Service (EaaS) solutions at no up-front cost for its customers, which include corporate and industrial clients, as well as municipalities, universities, schools and hospitals.
- Flexible addition of features via software protects investments
- New protection technologies prevent failures with distributed power supply
- Seamless integration in digital environments
With the new 3WA series, Siemens Smart Infrastructure is updating its Sentron portfolio of air circuit breakers. As a core element of low-voltage switchboards, they reliably protect electrical installations in buildings, infrastructures and industrial facilities from damage caused by short circuits, ground faults or overload faults. At the same time, the new 3WA circuit breakers meet all low-voltage power distribution requirements in digital environments. They support software-based planning and engineering, digital testing and monitoring, and seamless integration in automation and IoT systems. For the first time, upgrades can be completed 100 percent digitally. Users simply download new features from the Internet and add them using an app.
- Hydrogen production solely from renewable energy
- Exclusive hydrogen source for northern Bavaria and the border region in Czech Republic
- Cross-sector use of renewable energy as a model for the future
Siemens Smart Infrastructure and WUN H2 GmbH
signed a contract to build one of the largest hydrogen production plants in
Germany. It will be built in Wunsiedel in the north of Bavaria. With a power
intake of six megawatts in the initial development phase, the plant will run
solely on renewable energy and will be CO2-free. The electrolysis
plant from Siemens Energy will have the capacity to produce over 900 tons of
hydrogen per year in this first phase. When fully expanded, it will be able to
supply up to 2,000 tons. Groundbreaking is scheduled for the end of this year
and commissioning at the end of 2021.