- Railsystems RP GmbH orders two locomotives from Siemens Mobility
- Sustainable concept: a combined diesel and electric locomotive
- Delivery at the end of 2020
Railsystems RP GmbH has ordered two Vectron Dual Mode locomotives from Siemens Mobility, marking the first order for the new locomotive that can be operated either as a diesel or electric unit. Siemens Mobility first presented the concept at the InnoTrans 2018.
- VAG Nürnberg orders 12 Avenio trams
- Option for up to 75 additional trams
- Innovative interior concept for enhanced passenger comfort
VAG
Verkehrs-Aktiengesellschaft Nürnberg has ordered 12 four-section Avenio trams.
The contract includes options for a total of up to 75 additional trams. The
trams will serve on possible new lines or be used to expand VAG’s existing offering.
Commissioning is planned for the end of 2022.
- Third Mireo order from DB Regio
- Service in the Karlsruhe 7b network
- Passenger comfort and sustainably increased value over entire lifecycle
DB Regio, the regional transport business of Deutsche Bahn AG, has
ordered seven Mireo trains from Siemens Mobility. The trains will operate on
the regional express route between Karlsruhe and Heidelberg/Mannheim via
Bruchsal in the Karlsruhe 7b network. They will be built at the Siemens
Mobility plant in Krefeld, Germany, and their delivery is planned for the end
of 2022.
- New trend to supply renewable energy for mines as secure and cost-efficient alternative to fossil fuels
-
- Siemens' proven microgrid controller serves as technical basis for juwi's Hybrid IQ microgrid solutions
- Two projects in Australia successfully delivered, paving way for partners to roll-out solution in other countries
Siemens and the renewable energy developer juwi have joined forces to enter into a strategic technology partnership to focus on microgrids in the mining industry. A corresponding agreement was signed today. The two companies aim to roll-out and continually develop the advanced microgrid control system that enables the seamless integration of power from renewable energy to a mine's off-grid power supply. The Siemens Sicam based microgrid control platform is a proven and tested technology which is the basis for juwi's Hybrid IQ microgrid controller. juwi, on the other hand, brings industry-specific domain know-how and an excellent track record of planning and executing renewable energy projects at mine sites.
- Designed for future power networks and digital substations
- Enhanced cyber security and communications
- User-friendly interfaces and software
With the new Reyrolle 5 series of protection relays, Siemens is further developing its offerings for medium-voltage and industrial power networks. The protection, control, monitoring and measuring of power networks is a vital element in managing electrical assets, increasing reliability, sustainability and the safety of operating personnel. The first device applications of the new generation of protection relay will be overcurrent and earth fault protection and transformer protection in substations. It includes comprehensive functionality as standard, with enhanced process data such as faults, events and waveform records enabling the power network to be effectively managed. The small number of device variants allows easy ordering and efficient engineering while the improved hardware platform makes it even easier to operate and manage the protection relays.
- New Grid Diagnostic Suite offers unique comprehensive insights
- Gain a grid-wide view of energy automation systems
- Market launch of initially four cloud-enabled applications
- Enhances cost efficiency and availability of smart grids
- Support through digitalization in increasingly complex power grids
Siemens is presenting for the first time its new Grid Diagnostic Suite at the European Utility Week in Paris. The Grid Diagnostic Suite initially includes four cloud-based applications which collect data from new or existing field devices for protection, distribution automation and power quality. These data are stored and analyzed in the cloud. This requires almost no additional engineering effort. Distribution grid operators and operators of electricity grids in industrial parks can quickly tap into useful information from devices installed anywhere in the smart grid. This will enable grid faults, for example, to be detected at an early stage and quickly rectified. After information is collected, vulnerabilities can be identified, and necessary measures can be implemented before any damage occurs. In this way, Internet of Things (IoT) applications in the Grid Diagnostic Suite enhance the availability of power grids while enabling them to be operated cost-efficiently.
- Highly compact design, up to 110 kiloamps
- Maintenance-free up to 10,000 interrupting cycles at current of 15 kA
- Based on proven HB3 generator platform with vacuum switching tech
Siemens is expanding its HB3 generator circuit-breaker portfolio with a new compact version. The HB3-Compact (HB3-C) offers the possibility for vertical or horizontal mounting and uses maintenance-free vacuum switching technology. These features make it especially valuable for retrofit applications in power plants, where the highest security of supply is crucial, and space is limited due to existing installations. The new system will be presented for the first time at the European Utility Week 2019, taking place in Paris from November 12 to 14.
- First soft starter series with integrated Safe Torque Off function
- Enhanced protection when shutting down electric motors
- High functional density saves space and decreases cost
Siemens Smart Infrastructure expanded its soft starters portfolio for motors, with the launch of Sirius 3RW55 Failsafe and Sirius 3RW50. Soft starters ensure electrical motors used in industry and infrastructure are protected during startup and ramp-down. The Sirius 3RW55 Failsafe soft starters are the first to feature the integrated Safe Torque Off (STO) function. As specified in safety standards, the protection function for electrical drive systems ensures that torque-generating energy stops acting when motors are turned off, preventing an unwanted restart. Control panel manufacturers no longer require using separate individual components to have this function, which reduces the time and effort for wiring and maintenance works and saves space in the control cabinet. In addition, the switching time of the integrated solution is significantly shorter than for conventional, electromechanical components.
At this year’s European Utility Week (EUW) in Paris, Siemens Smart Infrastructure will demonstrate how it is driving energy intelligence across supply and demand. By helping shape the energy ecosystem across buildings, industry and the grid, Siemens is supporting government, cities and businesses with their sustainability goals. The company will focus on four topics that support the energy transition: sustainable grids, smart distribution, the Internet of Energy and grid edge.
- Campus Nyland test, training and signaling simulation center opens
- European Rail Traffic Management System (ERTMS) latest in intelligent infrastructure
- Nordlandsbanen will open first digital signaling railway in October 2022
Bane NOR and Siemens Mobility celebrated the opening of Campus Nyland, a test, training and signaling simulation center which will help the rail network operator prepare for the digitalization of the entire system. Norway has committed to becoming the first country to operate with a single digital interlocking and ERTMS signifies one of the country’s largest digitalization projects. In 2022, the first digital line, Nordlandsbanen, will open. In advance, the Campus Nyland center will prepare workers for working within the digital system, ERTMS. The intelligent infrastructure behind ERTMS will reduce operating costs and increase capacity throughout the network. In addition, it will enhance safety, with real-time visibility of trains across the network. When complete in 2034, the system will include 4,200 km of track and more than 350 stations.