Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Feature01 September 2021,
updated27 July 2022Siemens MobilityMunich
Siemens Mobility to install a 2,000 km state-of-the-art high-speed rail network that will connect 60 cities throughout the country with trains that can operate up to 230 km/h. The integrated system will create the 6ᵗʰ largest high-speed rail network in the world, and will provide 90% of Egyptians access to a modern, safe, and affordable transportation system. The fully electrified network will cut carbon emissions by 70% compared to current car or bus transport, further supporting Egypt’s efforts in transforming its mobility to a more sustainable one. Siemens Mobility will deliver 41 Velaro high-speed trains, 94 Desiro High Capacity regional train sets, and 41 Vectron freight locomotives. This contract also includes the development of eight depots and yards and 15 years of maintenance.
Infographic: A modern rail system
The Egyptian high-speed network will consist of three lines: One being the “Suez Canal on rails,” a 660 km line connecting the port cities of Ain Sokhna on the Red Sea to Marsa Matrouh and Alexandria on the Mediterranean. The second line will be about 1,100 km long and run between Cairo and Abu Simbel near the Sudan border, linking the mega city to rising economic centers in the south. The third line will cover about 225 km and connect the world heritage archeological sites in Luxor with Hurghada by the Red Sea. In addition, this rail link will significantly improve the efficiency and sustainability of freight transport for goods and materials between Safaga harbor and inland locations.
Press Release24 September 2024
Siemens Mobility presents first Velaro high-speed train for Egypt at InnoTrans, Berlin
Press Release28 May 2022
Siemens Mobility finalizes contract for 2,000 km high-speed rail system in Egypt
Press Release01 September 2021
Siemens Mobility Signs Historic Contract for Turnkey Rail System in Egypt worth USD 3 bn
Videos
The rail system will not only transform transportation, but also be very beneficial for Egypt’s society and environment. It will provide efficient, safe, and affordable transportation for all Egyptians, as well as goods across the country. It will establish Egypt as a regional leader for transportation and provide an additional boost to the economy. For the entire system, the consortium will directly create up to 40,000 jobs, with an additional 6,700 being initiated by Egyptian suppliers and indirectly through the wider Egyptian economy.
Siemens Mobility will deliver its Velaro high-speed trains, Desiro
high-capacity regional train sets, and Vectron freight locomotives. A safe and reliable signaling system based on the latest computer-based
interlocking technology and
European Train Control
System [ETCS] Level
2 will be installed, as well as the power supply system that delivers
efficient and continuous energy. Furthermore,
Siemens will provide and integrate the latest communications, safety and
security systems that will create a pleasant passenger experience.
Download Animated Train Footage and B-Roll