Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser
Copenhagen's S-tog on the path to automatic operation
Copenhagen's S-tog (commuter rail system) is the backbone of the capital's public mass transit network. It carries around 350,000 passengers a day - and that number is growing all the time. This reflects the growth in the metropolitan area around the Danish capital where more than one fifth of the entire population of Denmark now lives. So, in the space of six years, Siemens will equip Copenhagen's entire commuter rail network with the Trainguard MT train control system which uses Communications-Based Train Control (CBTC) to automate operation. This has made it possible to reduce train headways from 120 seconds to 70 seconds within the inner-city area.
The first phase; the newly opened 25 kilometer section of Line A runs from the suburb of Hillerod in the north to Jaegersborg east of the capital and will be used by more than 70.000 commuters a day. Once the complete network is open, up to 84 trains an hour will travel on the core network - equivalent to more than 1 million passengers per year. The remaining phases will enter passenger service in the coming years.

Press Pictures

First section of Copenhagen's S-Bahn now in service

In the Danish capital, Copenhagen, Siemens is currently equipping the entire 170 kilometers of the dual-track commuter rail network with a Communications-Based Control System. The project is divided into 6 phases. The first phase (opened February 2016); the newly opened 25 kilometer section of Line A runs from the suburb of Hillerod in the north to Jaegersborg east of the capital and will be used by more than 70.000 commuters a day.

In the picture: The operational control center in Copenhagen

Siemens rail technology reduces train headways Of Copenhagen's S-Bahn by around 25 percent

Copenhagen's S-Bahn is the backbone of the capital's public mass transit network. It carries around 350,000 passengers a day - and that number is growing all the time. So, in the space of six years, Siemens will equip Copenhagen's entire commuter rail network with the Trainguard MT train control system which uses Communications-Based Train Control (CBTC) to automate operation. This has made it possible to reduce train headways from 120 seconds to 70 seconds within the inner-city area. First section of Copenhagen's S-Bahn is in service since February 29, 2016.

In the picture: The operational control center in Copenhagen

First section of Copenhagen's S-Bahn now in service

Initially, the Copenhagen system will operate in semi-automated mode. This means that the S-Bahn trains will be controlled automatically to a large extent but there will still be driver involvement. Siemens will also supply electronic interlockings (Trackguard Sicas ECC), on-board units for a total of 135 S-Bahn trains as well as the operations control system (Controlguide OCS) that monitors traffic and controls interlockings and infrastructure.

In the picture: The operational control center in Copenhagen

Siemens rail technology reduces train headways Of Copenhagen's S-Bahn by around 25 percent

Copenhagen's S-Bahn is the backbone of the capital's public mass transit network. It carries around 350,000 passengers a day - and that number is growing all the time. So, in the space of six years, Siemens will equip Copenhagen's entire commuter rail network with the Trainguard MT train control system which uses Communications-Based Train Control (CBTC) to automate operation. This has made it possible to reduce train headways from 120 seconds to 70 seconds within the inner-city area. First section of Copenhagen's S-Bahn is in service since February 29, 2016.

In the picture: The operational control center in Copenhagen

Copenhagen's S-Bane network to get signaling from Siemens worth 252 million euros

Banedanmark, the Danish railway infrastructure developer and operator, has placed a contract with Siemens for the modernization of the complete signaling system of the Copenhagen commuter rail ("S-Bane") network. This contract is worth 252 million euros, making it the biggest rail automation order that Siemens has ever received. It calls for the supply and installation of the fully automatic Trainguard MT type train control system, Sicas type electronic interlockings, and switch machines. The equipment package also includes a brand-new operations control center. The first of six construction phases equipped with the new signaling system is scheduled to go into operation already before the end of 2014. The contract also includes maintenance services for 25 years.

From left: Morten Søndergaard (Programme Director Signaling Banedanmark), Jesper Hansen (CEO Banedanmark), Jochen Eickholt (CEO Siemens Business Unit Rail Automation), Jukka Pertola (CEO Siemens Danmark)

Further Information

Trainguard MT

The demand for public mass-transit transportation services is growing continuously. However, passenger capacity can seldom be expanded as generously as would actually be necessary. To continue to ensure the smooth running of mobility systems, on-track effectiveness and efficiency must be improved. The solution here is automation. With automation, the capacity of a metro line can be increased by up to 50 percent. Automated metro systems make it possible to realize short headway times of 80 to 90 seconds. Optimized acceleration, traction and breaking processes consume less energy. Depending on the degree of automation, power consumption can be reduced by up to 30 percent while simultaneously increasing train punctuality. On the basis of line data, the system calculates exactly how and at which point a train has to be accelerated and braked for it to arrive at the next station on time. The Siemens solution, Trainguard MT, is the most widely used system in the world today and is deployed by more than 25 metro operators, such as in São Paulo, Barcelona, Algiers, Paris and Guangzhou.

Press Pictures

Trainguard MT provides highest flexibility for mass-transit systems

The modular train control system Trainguard MT provides the signaling basis for reliable and efficient mass-transit systems. Trainguard MT includes functions for monitoring, implementation, and control of the entire operating sequence. It can be implemented in different degrees of automation, e.g., semiautomatic operation, operation under driver control, and driverless operation.

Trainguard MT starts passenger service

Trainguard MT comprises all functions for monitoring, performing and controlling the fully automatic operational process. Continuous data communication takes place between the control center, the trackside equipment and the trains via a WLAN radio network. This makes it possible to pinpoint the exact location of each train within the railway network. The CBTC-solution Trainguard MT is the most extensively deployed automatic train control system and is used by more than 20 metro operators around the world.

First metro line in Algerian capital to start passenger service

In the capital Algiers inaugurated the first metro line. Siemens, as the consortium leader, delivered the complete rail system as a turnkey project. The Siemens scope of supply comprised the automatic train control system Trainguard MT CBTC, the radio communication system Airlink and the train location system Digiloc. Siemens also installed the telecommunication system, the traction power supply, the trackworks and the ticket vending system. The operations control center was also equipped with technology from Siemens. The company was also responsible for the project management and the entire project planning. Consortium partners were Construcciones y Auxiliar de Ferrocarriles S.A. (CAF) and Vinci Construction.

Further Information

Contact

Silke Thomson-Pottebohm

Siemens Mobility GmbH

+44 7808 822780

Link to this page
www.siemens.com/press/cbtc-copenhagen