Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release18 February 2019Digital Factory Nuremberg
Siemens to showcase new applications for machine-level edge computing

The picture shows new applications for Sinumerik Edge, the machine-level platform specifically targeting the machine tool industry.
The new edge application Analyze MyWorkpiece /Capture allows machine tool users to record all kinds of workpiece, tool and tool path data with a high temporal resolution. Additional data such as drive currents, control deviations or spindle torque can also be recorded. The user is able to determine which data should be captured and how, for instance only for selected machining steps or from specific threshold values. The recorded data can subsequently be imported into the CNC shopfloor management application Analyze MyWorkpiece /Toolpath, where it can be visualized and analyzed. The recorded position data can be used to reconstruct a 3D representation, and additional measurement values can also be depicted with color coding as a fourth dimension using the component topology. The color coding enables functions such as the identification of deviating path velocities. The color-coded visualization of path curvature offers further scope for analysis. Fundamentally, the applications enable target data – generated for instance by CAM – to be compared to data recorded during the actual process. As the resulting findings enable optimization of the CAD/CAM model and the generated NC program, the Analyze MyWorkpiece /Toolpath application helps provide the assurance of quality right from the very first produced workpiece. The improved degree of transparency enables the deduction of wide-ranging findings which can be used to bring about an overall improvement in process quality and process development.
The edge application Analyze MyMachine /Condition captures a mechanical fingerprint of the machine tool. Flexibly configurable measurement series can be used to capture a variety of parameters such as rigidity, friction and reverse backlash in the individual axes. By visualizing the measured results and comparing them to reference data, an overall improvement of machine tool condition transparency is achieved. The early identification of non-conformance made possible by the application allows optimized machine operation and reduced machine downtimes. Condition-dependent maintenance also makes for optimized processes and cost savings. Improving and correcting machine parameters such as control variables can prevent any potential loss of quality in running production. This is another Sinumerik Edge application which significantly improves machine tool availability and consequently also productivity.
With its Sinumerik Edge portfolio, Siemens is providing a machine-level platform designed specifically for machine tools featuring a range of software applications capable of capturing high-frequency data generated during machine tool operation, which is then processed, analyzed and forwarded to higher-level systems. Using the platform approach means that the edge applications offer practically unlimited scope in terms of their function within a secured ecosystem. Other benefits provided by the platform include simple connection to the Sinumeric controller, a security infrastructure and the facility for users to program their own edge applications. With its new edge applications Analyze MyWorkpiece /Capture and Analyze MyMachine /Condition as well as the Optimize My Machining /Trochoidal application designed to significantly extend tool life by means of trochoidal milling, which was unveiled back in September 2018, Siemens is now offering applications which address the three main value drivers of edge computing in the machine tool sector: Process quality, machine condition and productivity improvement.
For further information regarding the CNC-Shopfloormanagement Software, please see www.siemens.com/machinetools-digitalization
For further information on Siemens at the Hannover Messe 2018, please see www.siemens.com/press/hm19 and www.siemens.com/hannovermesse
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2019020156DFEN
Contact
Katharina Lamsa
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7975