Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release08 January 2019Siemens AGZug
Siemens inaugurates new campus in Zug
“Siemens is one of Switzerland's largest employers. We employ over 6,000 people
here, including about 300 apprentices said Joe Kaeser, Chairman of the Siemens
AG Managing Board. “Building Technologies with its headquarters in Zug will benefit
more from digitalization than virtually any other industry. Next year, building
technology will become a core element of the new operating company Smart
Infrastructure (SI). Its global headquarters will then also be in Zug.”
Zug has been home to Siemens Building Technologies since 1998, when Siemens
took over the industrial activities of Elektrowatt AG. “With our investments in
research and development, we are using the opportunities of digitalization to
steadily evolve into a smart building company,” explained Matthias Rebellius, CEO
of Siemens Building Technologies. “We offer a full range of building technologies for
fire detection, security and automation solutions to optimize sustainability, total cost
of ownership and the user experience in buildings. Smart buildings are based on
comprehensive analytics and use of digital building data.” Rebellius called the campus a reference project that illustrates the opportunities of digitalization in
building technology, energy efficiency and future-oriented working. “A smart building
is flexible, it learns from previous interactions and it continually adapts to the needs
of building users, thus actively contributing to their success.”
Construction of the office and production buildings began in May 2016 and was
completed in July 2018. The Siemens Zug campus is one of the first new projects to
use Building Information Modeling (BIM) for design and construction. The digital twin
– a 3D model of the building, enhanced with technical information relevant for later
operations – is the foundation for efficient, cost-optimized and forward-looking
building management.
The campus complex is equipped with building automation, security and fire safety
technology from Siemens BT. Particular emphasis was placed on sustainability and
energy efficiency of the buildings. The office building meets the highest
requirements of the LEED standard, earning it a Platinum certification; the
production building meets the criteria for LEED Gold certification. An integrated
building automation system with energy optimization based on the Desigo CC
integrated building management platform controls the energy consumption and all
the disciplines in the buildings. Energy-efficient heat pumps use water from Lake
Zug as a heat source and for direct cooling. The campus buildings do not need fossil
fuels to generate energy. The heating, ventilation and air conditioning systems are
equipped with heat and cold recovery systems. Even the compressed air systems in
production have an energy recovery system for water heating. The buildings have
green roofs, and the office building uses approximately 1,500 m3 of rainwater. A
photovoltaic system on the roof of the production building will go into operation in
the spring of 2019
With its 56 x 56 meter footprint, the seven-story office building can accommodate
1,000 employees. It has 32,000 m2 of gross floor space, including 18,400 m2 of
office space and 11,000 m2 in the two-story underground garage with 250 parking
spaces. The building has a height of 25 meters.
The three-story production building has a height of 16 meters, a footprint of 125 x 50
meters and two production floors. The second upper floor of the building has 120
office spaces as well as additional space for occupational training and a laboratory.
Delivery docks, nitrogen tanks and waste containers are integrated into the building to minimize noise for the neighboring residential area and to make it architecturally
attractive
The campus also includes an existing office and production building, scheduled for
modernization in 2021. Beginning in late 2022 it will house the approximately 450
employees of BT research and development. The city of Zug is taking over the
former Siemens office building.
The Siemens Zug campus is the international headquarters of the Siemens Building
Technologies (BT) Division. The Siemens Building Technologies Division is not only
a leading developer and supplier of products, systems solutions and services in
building automation, energy efficiency, fire safety and security, but also a pioneer in
building digitalization. In 2018, BT had more than 29,000 employees in more than
400 locations worldwide and posted sales totaling 6.6 billion euros. Building
Technologies has been located in Zug since the takeover of the industrial activities
of Elektrowatt in 1998. More than 1,700 employees work for BT in Zug.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Elisavet-Vasiliki Sachinidou
Siemens S.A.
Agisilaou 6-8
Marousi, Athens
Marousi, Athens
Tel.: 210 68.64.267