Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Lehdistötiedote01 March 2024Smart InfrastructureZug
Siemens introduces one of the world’s most innovative circuit protection devices
SENTRON ECPD (Electronic Circuit Protection Device)
SENTRON ECPD enables completely new
approaches in electrical planning, maximizing safety, flexibility and
delivering enormous space and energy savings compared to conventional
solutions. “For the first time in the history of circuit protection, it is
possible to benefit from several functionalities in one product and to activate
them as required by the individual application or adapt them if needed. All of
this combined with the solid-state switching technology enables up to a
thousand times faster, wear-free switching,” added Matthé.
Ultra-fast
Circuit protection devices are central
components of every electrical installation. If certain load current limits are
exceeded, these devices disconnect the individual loads to protect people and
systems from damage. In the event of a short circuit, for example, this type of
disconnection occurs in commercially available circuit breakers in two to three
milliseconds.
In comparison, SENTRON ECPD disconnects up to
a thousand times faster, minimizing the occurring short-circuit energy. This
ensures maximum safety for people, systems, and electrical equipment. SENTRON
ECPD also offers wear-free switching, which increases the service life of
systems and reduces maintenance and repair costs. In addition, the integrated
cyclical self-test (including the integrated RCD function) raises safety to an
entirely new level not covered by current concepts.
Multifunctional and parametrizable
The smart SENTRON ECPD offers more
functionalities in one compact design, saving space and costs. The range of
functions can be customized as required. New functions can be easily activated
on the SENTRON ECPD without having to purchase a new device and functionally adapt
it into the circuit. The SENTRON powerconfig app makes this task easy and
convenient.
SENTRON ECPD can be adjusted as required and
adapts perfectly to the requirements of the application, for example with
regard to rated current, tripping limits or behavior. These properties offer
major planning and cost advantages. For example, circuits can simply be
designed based on the rated current of the loads instead of the significantly
higher inrush current peaks that occur briefly with certain load types, such as
LED lights. This reduces complexity as well as planning and installation
efforts and saves on materials such as copper.
Reducing operating costs and downtime
SENTRON ECPD offers full transparency on
energy consumption in the final circuit through radio-based communication with
the SENTRON Powercenter 1000 and 3000 gateways. This enables measures to
optimize systems and processes, for example as part of energy management in
accordance with ISO 50001, which in turn allows for efficient reductions in
energy and operating costs.
For the first time, it is possible to perform
detailed condition monitoring of the applications at the final circuit level.
This substantially increases availability and operational reliability. The
large volume of measurement data enables the detection of irregularities and
deviations and creates a reliable planning basis for preventive maintenance.
SENTRON ECPD can be easily integrated into higher-level systems by using the
open Modbus TCP standard.
SENTRON ECPD makes it possible to carry out
remote diagnostics and remote switching during normal operation as well as in
the event of a fault. This offers significant benefits, especially for remote
applications without direct on-site support. In addition, it is easier to
localize and identify faults by differentiating the cause of the fault.
Sustainable
SENTRON ECPD combines multiple product
functions in one device. Depending on the application, this allows savings of
up to 80 percent on electronics, 90 percent on metals and 90 percent on
plastics. Overall, SENTRON ECPD is approximately 90 percent lighter than the
devices otherwise required. Compared to solutions based on today’s conventional technology, SENTRON
ECPD also requires up to 80 percent less space in the distribution board,
eliminating the need for costly structural measures.
For further information on the ECPD, please see
www.siemens.com/sentron-ecpd
For further information on Siemens Smart Infrastructure, please see
www.siemens.com/smart-infrastructure
www.siemens.com/smart-infrastructure
For this press release
Follow us on X
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2023, the business had around 75,000 employees worldwide.
Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare.
In fiscal 2023, which ended on September 30, 2023, the Siemens Group generated revenue of €77.8 billion and net income of €8.5 billion. As of September 30, 2023, the company employed around 320,000 people worldwide. Further information is available on the Internet at www.siemens.com.
In fiscal 2023, which ended on September 30, 2023, the Siemens Group generated revenue of €77.8 billion and net income of €8.5 billion. As of September 30, 2023, the company employed around 320,000 people worldwide. Further information is available on the Internet at www.siemens.com.