Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release26 February 2018Process Industries and DrivesNuremberg
Upgraded power supply system now protects against hour-long power failures

The DC UPS module can be simply integrated into the system network of the Sitop PSU8600 using the System Clip Link. The battery module is installed by means of wall mounting outside the network and connected to the UPS8600 over a plus and minus wire and the two wires of the Energy Storage Link. This allows the system to automatically detect the battery type and diagnose the battery charge status. The smart battery management system permits temperature-led charging, which helps to extend the service life of the battery. The battery modules are fitted with lead (PB) or lithium iron phosphate (LiFePO4) batteries with a capacity of 380 Wh (Watt hours) and 264 Wh respectively. Users are able to connect up to five BAT8600 battery modules to one UPS8600 to further increase the mains power failure bridging time. The BAT8600 battery module using lithium technology offers a particularly long service life, even at higher ambient temperatures.
The DC UPS is able to communicate with practically any automation system at any time through the base PSU8600 module, which has Profinet and OPC UA capability. Users can respond directly to messages and diagnostic information about the operating mode (mains or buffer operation), charge status, buffer readiness, or the need to change a battery. Integration in the network allows several PCs to be safely powered down with the UPS8600.
Engineering takes place with the utmost convenience in the TIA Portal, while diagnostic functions use WinCC Faceplates or the Simatic PCS 7 Library. For open integration over Ethernet or OPC UA, new software is currently in preparation which enables convenient system-independent engineering, operation and observation.
For this press release

Event: Siemens at the Hannover Messe 2018
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616