Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Totally IP65 protected Comfort Panels for operator control and monitoring

The picture shows the new Simatic HMI Comfort Panel for operator control and monitoring.

The new Simatic HMI Comfort Panels PRO with total IP65 degree of protection have brilliant, continuously dimmable widescreen displays with 16 million colors and up to 170 degree angle of vision. The nonreflecting glass front has a modern design with a scratchproof, chemical resistant surface that allows operation with gloves. The Comfort Panels PRO are equipped with an integrated system card for automatic backups, and are also suitable for energy management directly on the machine, for example with Profienergy. Harmonized interaction with the Advanced Controllers Simatic S7-1500 and the use of conventional standard connectors for the cabling enable operator control and monitoring solutions to be realized especially economically. The mechanical design features adapters for flexible cabinet-free mounting on conventional stand or support arm systems. The individual mounting and placing options offer the operator a very high level of convenience and always an optimal view of the panel and visualization.
The Simatic HMI PRO series offers additional add-on system components for customized function and operation enhancements. The standard system – consisting of basic unit, expansion components, mounting adapter, and optional keyboard and keyboard shelf – allow customized, flexibly adaptable operator control and monitoring solutions. The devices are distinguished by easy mounting, quick commissioning and efficient engineering, and offer many years of cost-effective, safe and reliable operation. Siemens won the iF Design Award 2017 for the innovative system concept of the Simatic HMI PRO series.

For further information, refer to www.siemens.com/ip65-hmi-devices
For further information on Siemens at the Hannover Messe 2017, please see www.siemens.com/press/hm17 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2017040205DFEN

Contact

Gerhard Stauss

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7945