Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release07 August 2024Digital IndustriesNuremberg
Sinumerik 828D with new hardware and digital twin for more flexibility, sustainability, and cybersecurity
Sinumerik 828D PPU271.5, Sinumerik 828D PPU270.5 and redesigned operating concept Sinumerik 828D MCP
Run MyVirtual Machine available for Sinumerik 828D
The
new processor units allow the Sinumerik 828D to be upgraded to software version
5.24, paving the way for Sinumerik Run MyVirtual Machine. As with Sinumerik
One, the digital native CNC, Run MyVirtual Machine allows NC programs to be
created, validated, and optimized using a digital twin of the machine without
interrupting production. This reduces the set-up time on the real machine by up
to 20 percent and minimizes production risks. In addition, the working area of
the machine, clamping, tool, and material removal can be visualized in detail
in all phases of the NC program. Potential collisions can therefore be recognized
and eliminated in advance. Training new employees with Run MyVirtual Machine
also saves machine time and minimizes the risk of damage due to incorrect
operation or programming errors.
Redesigned operating concept Sinumerik 828D MCP
The
redesigned Sinumerik 828D MCP operating concept is being introduced to match
the new generation of processor units. This launches a more intuitive machine
operation for the Sinumerik 828D from Siemens, which offers CNC users greater
user-friendliness, efficiency, and flexibility. The redesigned Sinumerik 828D
MCP operating concept includes significantly larger and innovatively designed
control panels with 12.1-inch and 15.6-inch screens as well as mechanical keys.
Create MyHMI/3GL can also be used to further customize the user interface for
specific areas of application.
Sinumerik 828D PU272.5
Enhanced connectivity, more transparent energy efficiency, and improved security functions
The
new processor units have an X120 interface, which enables connection to
external devices like Sinumerik HT (Handheld Terminal) 10 or edge devices. This
extends the range of applications and increases productivity. The Ctrl-E key
combination also provides the user with a comprehensive analysis function that makes
energy consumption transparent. In the area of cybersecurity, the new processor
units offer security functions like a security archive, user management, and
certificate storage, which offers protection from manipulation and product piracy.
With
the new hardware and the associated new software for the Sinumerik 828D,
Siemens is again paving the way for digital twins to acquire greater
flexibility, productivity, and sustainability. At the same time, the range of
applications for the control of turning, milling, and grinding technology is
expanding to the areas of power and energy, electronics and 5G, automotive, and
more.
For this press release
Links
Follow us on social media
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions, and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has employed around 72,000 people internationally.
Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare.
In fiscal 2023, which ended on September 30, 2023, the Siemens Group generated revenue of €77.8 billion and net income of €8.5 billion. As of September 30, 2023, the company employed around 320,000 people worldwide. Further information is available on the Internet at
www.siemens.com.