Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release04 April 2017Process Industries and DrivesNuremberg
Siemens supplies digitalization package for the next Simotics SD motor generation

The picture shows Simotics SD motors.
The new compact, highly space-saving Simotics SD motors are available in sizes 315 and 355. The new design with its exceptional heat dissipation complies with the stringent efficiency demands of efficiency classes IE3, IE4 and IES2 without compromising power density. The new, highly flexible terminal box concept allows the motors to be simply adapted to any mounting location. Siemens offers highly favorable delivery periods of between just 15 and 20 working days.
In future, the new Smart Motor Concept will enable simple analysis of motor status data in MindSphere. Depending on their length of service and the loads placed on them, drive components such as motors are exposed to varying levels of wear and continuous abrasion. The strains can often remain invisible to the naked eye for quite some time, leading to outages and unscheduled downtimes which can result in incalculable financial losses. Smart Motor Concept and MindSphere enable the relevant motor data to be accessed anywhere around the world. The transparency gained using this technology enables improved productivity throughout the entire customer process, for example as a result of increased availability, improved performance and optimized servicing activity.
The DataMatrix code placed on the motor as standard enables machine-readable motor identification and – for instance using a smart device – rapid access to motor-related information such as the electronic rating plate, with a range of associated benefits including simpler commissioning and spare part order placement. The use of a digital twin also makes available valuable aids such as 2D drawings and 3D models.
For further information on topic of Simotics SD, please see
http://siemens.com/simotics-sd-nextgeneration
http://siemens.com/simotics-sd-nextgeneration
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2017040222PDEN
Contact
Stefan Rauscher
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7952