Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release21 June 2022Siemens AGZug
Siemens to show integrated technologies accelerating decarbonization of buildings

Green hydrogen is the future: At MCE 2022, Siemens will be showing solutions for OEMs that are fit for a pure hydrogen market.
This year's highlights from
Siemens include a newly developed application for residential boilers that
supports operation with hydrogen. It allows OEMs to develop advanced,
user-friendly solutions that meet future energy requirements and are ready for
the gradual transition to a pure hydrogen (H2) market. This
application for residential boilers is part of a comprehensive hydrogen
portfolio that supports the European Green Deal, a set of policy initiatives
aimed at making the European Union carbon-neutral by 2050.
Greater heating efficiency is also provided by another innovation Siemens is showing at MCE: an intelligent and fully digitalized heat interface unit (HIU) control solution. HIUs are typically installed in multi-family apartment buildings in which a central heating plant provides heating and in some cases hot domestic water to all units. State-of-the-art HIU controls from Siemens allow control and remote metering/billing for multiple zones on an individual apartment level. This increases transparency and efficiency of energy usage. For maximum efficiency, Siemens combines HIU with heat recovery ventilation (HRV). As a result, heating costs can be significantly lowered. Its cloud connectivity ensures full transparency on energy flow and operating status. In addition, the unit supports heating and hot water circuits, and it can be connected to Climatix heat recovery systems.
The new LMV6 burner management
system provides a significant boost in efficiency for medium and high capacity burners. This means less fuel is burned for the same amount of energy, compared
to other burner management solutions. The control unit (AZL6) redefines the
benchmark for HMIs (Human Machine Interface) in the burner business. Its graphical display allows straightforward burner
commissioning with clear text information in multiple languages and easy,
guided commissioning for fast burner start-up.
With Adaptive Flow Optimization,
Siemens is also presenting a new function at the MCE for the Intelligent Valve,
the self-optimizing dynamic valve with cloud connection. Adaptive Flow
Optimization eliminates pressure fluctuations, ensures stable room temperatures
and high comfort, and saves up to 30 percent energy.
The latest development in Climatix
technology focuses on renewable heat generation. Thanks to a new, customizable
user interface, heat pumps can now be commissioned, operated and maintained
quickly and efficiently via mobile app.
In addition to these highlights,
Siemens will show a wide range of building automation solutions for controlling
and managing cooling, heating, humidity, and CO2, as well as
lighting and shading at Booth P41 R42 in Heating Hall 7.
For further information on Siemens at MCE, please see
www.siemens.com/mce
www.siemens.com/mce
For further information on Siemens Smart Infrastructure,
please see
www.siemens.com/smart-infrastructure
www.siemens.com/smart-infrastructure
For this press release
Follow us on Twitter at
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2021, which ended on September 30, 2021, the Siemens Group generated revenue of €62.3 billion and net income of €6.7 billion. As of September 30, 2021, the company had around 303,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.