Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens provides access to unused field data from production for the integration of IT and OT

Field Data Enablement via hardware or software

FDE will be available beginning in April as a hardware solution or as an app: Both can be used independently. The SIMATIC FDE Gateway can be used to access devices at the field level that aren’t connected to the automation or controller by a permanent bus connection. The Field Data Enabler PROFINET app can be installed on a SIMATIC IPC. Data acquisition occurs in parallel to automation via an existing PROFINET connection. The app can also use this connection to directly access all data from field devices that are connected to the decentralized I/O system via IO-Link. This is how OT data, such as valuable status information from the sensor, can be made available to IT. The convergence of IT and OT enables secure, data-driven decisions.

Easy implementation in green- or brownfield

Field Data Enablement can be easily integrated in existing systems, because no additional sensors need to be retrofitted. Operators can use sensors they already use for automation in the OT layer for further analysis in the IT environment. FDE is easy to configure with no need for programming. Instead of the programming necessary for IoT solutions, all that’s needed is the configuration of the existing information. In addition, parameters like context and semantic reference can be reused, and no redefinition is necessary. This is how Field Data Enablement is advancing the fusion of OT and IT in plants of all sizes.
For more information on SIMATIC Field Enablement please see www.siemens.com/fde
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 72,000 employees internationally.
Read more
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: HQDIPR202303026656EN

Contact

Fabiane Hörmann

Siemens AG

+49 15238919337