Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release21 July 2020Smart InfrastructureZug
Siemens presents new state-of-the-art actuator line for small valves
Flexible, fast and space-saving installation
All new actuators are delivered pre-configured and are ready for immediate installation. The newly introduced IP54 protection rating accommodates all installation directions, including overhead installations, for even greater versatility. In addition, the new products offer automatic hub adaptation, ensuring that everyvalve-actuator combination is perfectly matched. Increased comfort and additional energy-saving potential are achieved in combination with pressure-independent control valves (PICVs). PICVs prevent oversupply and reciprocal hydronic interference, ensuring a balanced hydronic system under all load conditions.
The new LED status display on the SSA actuators ensures fast and error-free commissioning. It shows the position of the valve and different operating states and helps users with various functions, such as self-calibration.

New features for customized applications
The actuators are particularly cost-efficient because they accommodate the needs of users, allowing them to buy actuators with just the functions required for their projects. Users can choose between a basic and a premium version with feedback signal and manual adjustment. The feedback signal enables early fault detection and fast elimination of inconsistencies, helping prevent system downtime. The technology of the actuator is with <30 dB optimized for silent applications making it one of the quietest products in this segment. This makes the new SSA actuators ideal for use in hotels, hospitals and libraries. Since they are 100% backward- compatible, old actuators can easily be replaced during ongoing operations.
For more information on Siemens Smart Infrastructure, see
www.siemens.com/smart-infrastructure
www.siemens.com/smart-infrastructure
For further information on the Acvatix portfolio, please see
www.siemens.com/acvatix
www.siemens.com/acvatix
For this press release
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 72,000 employees worldwide.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed companies Siemens Energy, the global energy business of Siemens, and Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the energy systems of today and tomorrow as well as the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy (as part of Siemens Energy), Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: HQSIPR202007205946EN
Contact
Katharina Sipura
Smart Infrastructure
Theilerstrasse 1a
6300 Zug
Switzerland
6300 Zug
Switzerland
+41 796507005