Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release28 September 2015MobilityMunich
Siemens to modernize weir complexes in the Netherlands

Siemens to modernize weir complexes in the Netherlands
The weir complexes on the Nederrijn and Lek rivers are 50 years old and will undergo a major renovation. Replacing technical installations and moving systems, as well as introducing Remote Operation, will ensure that the weir complexes can continue to perform their important work safely and reliably in the years to come. The weir at Driel is known as 'the tap of the Netherlands'. It distributes the water that flows in from the Rhine between the rivers, which also ensures that enough fresh water continues to flow into the IJsselmeer. The IJsselmeer is the largest freshwater basin in the Netherlands and is essential to the provision of potable water.
Weir complexes were built between 1960 and 1970 at Hagestein, Driel and Amerongen to regulate the water discharge of the various rivers in the northern part of the Netherlands and keep the water level of the Nederrijn river constant. If too much water is discharged by the Rhine, the weirs are opened and the water can flow to the sea at a much faster pace.
The weirs are semi-circular visor weirs with a width clearance of 50 meters and a height of about nine meters. Every complex also has a lock that allows ships to pass when the weirs are closed. The weirs in the Nederrijn and Lek rivers present a major obstacle for fish. They completely block the river. For this reason a fish way was built alongside the weirs. The fish way allows salmon and sea trout to reach their spawning grounds via the Lek and Nederrijn rivers.
Waterways are important for the Netherlands. No other country has such a dense network of waterways, which stretches over 5000 kilometers. They form a complete water system. The Dutch authorities are making great efforts to modernize this important part of the traffic infrastructure, using the latest technology, and to make water transport operations run more smoothly and efficiently. To ensure safe round-the-clock operations, several weirs and locks will now be linked up technically and controlled and monitored centrally. On-site camera systems and video panels in the control rooms ensure that operators have a direct view of the situation at the lock systems.
Links
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is no. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 343,000 employees worldwide on a continuing basis. Further information is available on the Internet at www.siemens.com.
Contact
Katharina Ebert
Siemens AG
Otto-Hahn-Ring 6
81739 Munich
Germany
81739 Munich
Germany
+49 (89) 636-636802