Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens Mobility receives approval for Vectron Dual Mode

“The Vectron Dual Mode enables our customers to provide sustainable and cost-effective rail freight transport. As an alternative to conventional diesel locomotives, the Vectron Dual Mode offers the best of two worlds: It operates in electric mode on electrified rail routes to save fuel and reduce emissions and maintenance costs, and can switch to diesel operation on sections without overhead lines, eliminating the need to change locomotives,” said Albrecht Neumann, CEO Rolling Stock at Siemens Mobility.
The German rail network is currently around 60 percent electrified, and the Siemens Mobility locomotive can operate through gaps in the system’s electrification without requiring a change of locomotives. At the same time, metropolitan areas and large cities, which often have an electrified network, are spared emissions.
The Vectron Dual Mode locomotive is based on the proven Vectron platform and components. It has a track gauge of 1,435 mm and weighs 90 tons. The locomotive is designed to operate on a 15-kV AC voltage system and is equipped with a PZB train protection system. Regardless of its operating mode, the locomotive has 2,000 kW traction power at the wheel rim. The fuel tank has a volume of 2,600 liters. The locomotive has a top speed of 160 km/h. 

This press release and additional information are available at www.siemens.com/press/vectron

For this press release

Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2019, which ended on September 30, 2019, the former Siemens Mobility Division posted revenue of €8.9 billion and had around 36,800 employees worldwide. Further information is available at: www.siemens.com/mobility.
Read more
Reference Number: HQMOPR202011046050EN

Contact

Eva Haupenthal

Siemens Mobility GmbH

Otto-Hahn-Ring 6
81739 Munich
Germany

+49 (89) 636-24421