[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release05 November 2020Siemens Mobility GmbHMunich
Siemens Mobility receives approval for Vectron Dual Mode
Over 100 combined diesel and electric locomotives already ordered
Sustainable and cost-effective solution for freight transport in Germany
The Vectron Dual Mode locomotive from Siemens Mobility received authorization for operation in Germany from the Federal Railway Authority (EBA) on October 29, 2020. To date, Railsystems RP, Mindener Kreisbahnen GmbH, and Stern & Hafferl have ordered the Vectron Dual Mode. The Siemens Mobility Test Center in Wegberg-Wildenrath has also ordered a locomotive for delivery trips. The dual mode locomotives ordered by DB Cargo in September will also benefit from the authorization.
Over 100 combined diesel and electric locomotives already ordered
Sustainable and cost-effective solution for freight transport in Germany
The Vectron Dual Mode locomotive from Siemens Mobility received authorization for operation in Germany from the Federal Railway Authority (EBA) on October 29, 2020. To date, Railsystems RP, Mindener Kreisbahnen GmbH, and Stern & Hafferl have ordered the Vectron Dual Mode. The Siemens Mobility Test Center in Wegberg-Wildenrath has also ordered a locomotive for delivery trips. The dual mode locomotives ordered by DB Cargo in September will also benefit from the authorization.
“The Vectron
Dual Mode enables our customers to provide sustainable and cost-effective rail
freight transport. As an alternative to conventional diesel locomotives, the
Vectron Dual Mode offers the best of two worlds: It operates in electric mode on
electrified rail routes to save fuel and reduce emissions and maintenance
costs, and can switch to diesel operation on sections without overhead lines,
eliminating the need to change locomotives,” said Albrecht Neumann, CEO Rolling
Stock at Siemens Mobility.
The German rail network is currently around 60 percent electrified, and the Siemens Mobility locomotive can operate through gaps in the system’s electrification without requiring a change of locomotives. At the same time, metropolitan areas and large cities, which often have an electrified network, are spared emissions.
The Vectron Dual Mode locomotive is based on the proven Vectron platform and components. It has a track gauge of 1,435 mm and weighs 90 tons. The locomotive is designed to operate on a 15-kV AC voltage system and is equipped with a PZB train protection system. Regardless of its operating mode, the locomotive has 2,000 kW traction power at the wheel rim. The fuel tank has a volume of 2,600 liters. The locomotive has a top speed of 160 km/h.
Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2019, which ended on September 30, 2019, the former Siemens Mobility Division posted revenue of €8.9 billion and had around 36,800 employees worldwide. Further information is available at:
www.siemens.com/mobility.