[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release19 January 2024Siemens MobilityMunich
Siemens Mobility delivers first 70 Mireo
regional and long-distance trains to ÖBB
First call for 70 trains from the 2023
framework agreement
Order worth more than €800 million
Consistent development of the Mireo
platform
Austrian Federal Railways (ÖBB) has ordered the first 70
trains from the framework agreement won by Siemens Mobility at the end of
summer 2023. The trains will be delivered in three different versions from late
2027 onwards. The trains are a further development of the in Europe successfully
established and proven Mireo electric multiple-units. Designed to operate at
speeds up to 160 km/h, the Mireos offer numerous amenities for passengers,
including air conditioning, WiFi service, barrier-free access, electrical plugs,
racks for skis and snowboards, capacity for buggies and wheelchairs near the
doors as well as space for bicycles. The cars will be wider than on previous
Mireos trains to further enhance the passenger experience of ÖBB customers.
And, for the first time, Siemens Mobility is designing the new trains with
inner bearing bogies as a single car concept.
First call for 70 trains from the 2023
framework agreement
Order worth more than €800 million
Consistent development of the Mireo
platform
Austrian Federal Railways (ÖBB) has ordered the first 70
trains from the framework agreement won by Siemens Mobility at the end of
summer 2023. The trains will be delivered in three different versions from late
2027 onwards. The trains are a further development of the in Europe successfully
established and proven Mireo electric multiple-units. Designed to operate at
speeds up to 160 km/h, the Mireos offer numerous amenities for passengers,
including air conditioning, WiFi service, barrier-free access, electrical plugs,
racks for skis and snowboards, capacity for buggies and wheelchairs near the
doors as well as space for bicycles. The cars will be wider than on previous
Mireos trains to further enhance the passenger experience of ÖBB customers.
And, for the first time, Siemens Mobility is designing the new trains with
inner bearing bogies as a single car concept.
Copyright @ÖBB
Michael Peter, CEO Siemens Mobility: “Siemens Mobility
and ÖBB have long enjoyed a strong and trusting partnership. We are especially
proud to deliver a further development of the Mireo platform to ÖBB as a single
car concept for the company’s new fleet. With their numerous innovations,
cross-border operating capability, and high level of passenger comfort and
convenience, the new Mireo trains will help make ÖBB’s local and regional
transport even more attractive.”
"With the additional 70 multiple-unit trains, we are
consistently continuing our investment programme in a modern fleet. The new
trains have a speed of 160 km/h and offer increased passenger comfort,
barrier-free boarding, the option of transporting bicycles and Wi-Fi. In
addition, a special focus was placed on efficient energy consumption," emphasizes
ÖBB CEO Andreas Matthä.
The order consists of eleven 73-metre-long local trains and
28 106-metre-long trains for use in various federal regions. 31 trainsets with
a length of 106 metres for long-distance transport within the Alps complete the
first call-off.
The most modern European Train Control System [ETCS] from
Siemens Mobility will be used for controlling the train. In conjunction with
the appropriate infrastructure, the system enables significantly shorter train
intervals, which is an important economic factor on particularly busy routes.
The Mireo’s lightweight construction and resulting low energy
consumption, as well as its air conditioning systems using a natural
refrigerant and a heat pump, ensure greater sustainability. The trainsets are
especially environmentally friendly thanks to their low energy consumption. The
car bodies are aluminum, and a new lightweight construction technology is also
used for the inner bearing bogies.
Austrian know-how provides greater comfort for passengers The SF7500 bogies, which were developed at the Siemens
Mobility competence center for train bogies in Graz and have long since proven
their worth internationally, will be used on the Mireos. In contrast to
previous Mireo trains, in which two cars share one so-called “Jacobs bogie”,
each ÖBB Mireo car has two bogies. Several of them throughout the train are
powered by high-performance traction motors, ensuring acceleration that is
optimally balanced between traction and energy efficiency. The bogies are designed
with inner bearings to save weight and space, and the extra space gained is
used for relocating other components beneath the car body. This improves the
train’s handling and gives passengers more room and an enhanced spatial
experience.
The Mireo trains will be built within our global network of train
manufacturing facilities. The state-of-the-art bogies will be manufactured at
the Siemens Mobility competence center in Graz.
Siemens Mobility is a separately managed company of Siemens AG. As a leader in intelligent transport solutions for more than 175 years, Siemens Mobility is constantly innovating its portfolio. Its core areas include rolling stock, rail automation and electrification, a comprehensive software portfolio, turnkey systems as well as related services. With digital products and solutions, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2023, which ended on September 30, 2023, Siemens Mobility posted revenue of €10.5 billion and employed around 39,800 people worldwide. Further information is available at: www.siemens.com/mobility