Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release18 May 2017Power and GasErlangen
Siemens launches new gas engine E-series with power output of 2 MW

The picture shows a gas engine ot the E-series with a power output of two megawatts.
In 2015 Siemens acquired Guascor engines and generator sets as part of the Dresser-Rand product portfolio. The name of these engines now includes "SGE," for Siemens Gas Engine. Legacy Guascor engines are recognized as robust and efficient machines that deliver heat and power and perform reliably in critical and demanding applications. These products are engineered and tested under rigorous conditions. With roots dating back half a century, approximately 4,700 Guascor engines are operating in more than 50 countries around the world. Siemens' expanded portfolio now ranges from 300 kW to 2 MW for the gas engines; 4 to 66 MW for industrial and aeroderivative gas turbines; and up to 425 MW for heavy-duty gas turbines.
The new E-series gas engine is based on the thermodynamic Miller cycle combustion technology that ensures high reliability, minimal emissions, and longer run times between service intervals. With a mechanical efficiency of about 47 percent and an electrical efficiency of 45.4 percent, the engine offers a high level of performance for both prime power generation and cogeneration applications. The new engine series' capacity to deliver on-site power, heat, and cooling for a wide variety of commercial, industrial, and municipal applications translates into an excellent cost-performance ratio. With more than 3,000 operating hours and comprehensive testing at Siemens' Engine R&D Center in Miñano, Spain, demonstrated a reliable, efficient engine with competitive capital and operating costs.
"The new E-series engine offers a more compact and efficient alternative to the 2-MW engines available in the power generation market today," said Eva Garmendia, product line manager. "We can also offer one of the shortest lead times in the industry, with just 24 weeks from concept to delivery of a complete gen-set."
The new engine series is the result of in-depth market research that identified key product benefits. "In turn, this new E-series gas engine offers our clients the best-in-class alternative on the market, highest efficiency, excellent reliability, proven technology, and the smallest footprint: 34.5 cubic meters," said Iñaki Iruretagoiena, R&D Director for Engines.
Siemens E-series engines are especially well-suited for renewable energy and waste-to-energy, industrial power generation and cogeneration, and combined heat and power (CHP) applications. By generating electricity on-site and recovering heat typically wasted in a conventional power plant, CHP technology reduces energy costs and carbon emissions.
CHP is a common application used by large building complexes, like the one planned for the Siemens Campus in Erlangen, Germany. The Erlangen Campus will create a new urban district and debut as Siemens' first CO2-neutral location worldwide. In collaboration with Erlangen's municipal utility, the campus will operate on a CO2-neutral basis, thanks to state-of-the-art building and energy technology. A decentralized energy system that uses a separate cogeneration system based on four new SGE-86EM engines will provide district heating and cooling for the campus. This system will be combined with a single concept in order to adapt to the existing energy infrastructure and will eliminate expensive development or expansion of the existing infrastructure. The units are expected to be delivered to the site in 2018.
For further information on Siemens Campus in Erlangen, please see www.siemens.com/press/siemens-campus
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Susanne Weissmann
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 18-85753