Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release28 August 2018Energy ManagementErlangen
Siemens launches Frequency Stabilizer to support power grids in milliseconds

The picture shows the Frequency Stabilizer to support power grids.
The missing link in the energy transition
Depending on the country, the frequency of an AC grid remains at a constant 50 Hertz (in Europe, for example) or 60 Hertz (in North America, for instance) when the quantity of electricity generated and consumed is in balance. Renewable energy, however, is only available in variable quantities, depending on the sun and wind. More and more producers are feeding power locally; the distances between the power generation site – on the open ocean, for example – and the main points of consumption inland often amount to hundreds of kilometers. If a large consumer is then added or removed, the frequency in the grid, begins to fluctuate. An underfrequency occurs, for example, if the load abruptly increases or power plant capacity is suddenly absent. "In the near future, power management systems alone will no longer be able to compensate for imbalances in power grids," says Mirko Duesel, CEO Transmission Solutions at Energy Management. "The innovative and economical SVC Plus FS solution is the missing link that can ensure the grid stability we all need in this era of transition to a new energy mix."
Greater inertia and more robust grids
Large conventional power plants have long played a key role in maintaining a power balance. With fossil fuels, the power can be increased and decreased as needed. The kinetic energy stored in the flywheels of generators, for example, can quickly equalize small deviations. The grid is in balance again within seconds. Experts call the energy stored in the generator's rotating masses "grid inertia." However, fewer and fewer large power plants are available to maintain the inertia. At the same time, more and more renewable energy is being fed into the grid. Stored-pump power plants can only react slowly to frequency drops. "To avoid costly outages, some power plants switch to the inefficient standby mode," says Alexander Rentschler, Head of Product Lifecycle Management at Siemens Transmission Solutions. "The SVC Plus FS will make grid operators independent of this. The solution makes the grid more robust, increases its inertia, and thus builds a bridge for the energy transition."
The benefits of supercapacitors
Supercapacitors store energy. Their charging mode is electrostatic, which means that electrons are moved instead of molecules. As a result, they are charged and discharged much faster than storage batteries. Siemens buys the supercapacitors from its Californian partner Maxwell Technologies and is responsible for managing the static var capacitors and supercapacitors, connecting to the grid, and integrating the system. The SVC Plus FS takes up approximately two-thirds less space in comparison with a battery storage solution at the reference power of 50 Megawatt.
The press kit for CIGRE 2018 is available at www.siemens.com/press/cigre2018
For further information on Division Energy Management, please see www.siemens.com/energy-management
For further information on CIGRE 2018, please see https://www.siemens.com/cigre
For this press release

Event: Siemens at CIGRE 2018: Unlock the potential of digitalization
Press Event
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Sabrina Martin
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 7-37168