Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release02 May 2017Power and GasErlangen
Siemens introduces 38-MW aeroderivative gas turbine for oil and gas industry

The rendering shows the lightweight architecture of the SGT-A35 RB gas turbine
This combination produces a compelling solution for the challenging requirements of offshore applications, like floating production, storage and offloading (FPSO) vessels. FPSO vessels have become increasingly popular as oil and gas production moves towards deep-sea regions and harsher offshore environments to capture stranded reserves. With higher output and power density than comparable products, the SGT-A35 RB turbine offers several cost-effective solutions for this and other challenging offshore applications.
The SGT-A35 RB gas turbine, previously known as the Industrial RB211-GT30, is based on the proven pedigree of the Industrial RB211 and Industrial Trent 60 gas turbines, built with Rolls-Royce Aero Engine technology. This trusted legacy, evolved over 40 years of technological advancements, has more than 800 installations worldwide exceeding 37 million operating hours. The SGT-A35 RB variant introduces a lightweight free-power turbine derived from Rolls-Royce aerospace and marine Trent, as well as Siemens Industrial Trent 60. All rotating components are proven by millions of hours accumulated in flight, as well as industrial and marine service.
The SGT-A35 RB gas turbine is available in 34 and 38 MW variants to match a range of application requirements. Both ratings are available for mechanical drive and 60 Hertz or 50 Hertz electrical generation. In this configuration, the gas turbine can directly drive a 2-pole A/C generator without the need for a gearbox. The thermal efficiency of the gas turbine exceeds 40 percent at ISO conditions. The performance is ideal for hot climates and at 30 °C, the gas turbine retains more than 90 percent of its ISO power output.
The Dresser-Rand package uses fit-for-purpose packaging features and configurable options proven across oil and gas applications. Its modular design facilitates easy maintenance and reduces downtime to maximize availability and reduce clients' operating expenditures. The package has also been designed to quickly exchange the complete gas turbine and power turbine. Over the years, the Dresser-Rand business has supplied more than 1,000 aeroderivative gas turbine packages to the oil and gas industry.
"With the highest power density in this class we help offshore operators with a significant challenge," said Judy Marks, head of New Equipment Solutions for the Dresser-Rand business. "With gas turbines used as prime movers in offshore installations, project developers can simultaneously reduce capital investment and increase production capacity to achieve desired returns."
For further information on the SGT-A35 RB gas turbine, please see www.siemens.com/sgt-a35-rb
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Susanne Weissmann
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 18-85753