Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release28 March 2019Energy ManagementErlangen
Siemens expands its portfolio for SF6-free medium-voltage switchgear

The picture shows the SF6-free medium-voltage switchgear 8DJH 12.
The medium-voltage switchgear in the 8DJH family meet all requirements for safe and economical grid operation: compactness, maintenance-free design, and a high degree of operating and personal safety as well as availability. These benefits are also retained in the factory-assembled, type-tested, and 3-pole metal-enclosed 8DJH 12 model. The hermetically tight, welded switchgear vessel makes the high voltage components of the switchgear insensitive to ambient conditions and tight to the ingress of foreign objects.
With the 8DJH 12 Siemens is also responding to new market requirements: The gas contained in the switchgear consists only of the natural constituents of ambient air and insulates the current-carrying conductors inside the housing. The use of "Clean Air" makes the switchgear easy to handle throughout its entire lifecycle.
The medium-voltage switchgear operates by remote control, has communication capabilities, and can be connected to IoT platforms like MindSphere, the cloud-based, open IoT operating system from Siemens as well as to other systems.
The 8DJH 12 is characterized by a rated voltage of up to 12 kilovolts, a rated short-term current of 20 kiloamperes, and 630 amperes of rated current.
Possible applications are local ring-main units, customer transfer substations and switching substations of energy providers as well as industrial and infrastructure facilities that want to use the proven properties of GIS switchgear in their grids along with insulating media free of fluorinated gas.
"I am pleased that the switchgear in the 8DJH product family have been winning over customers all over the world for more than ten years now," says Stephan May, CEO of the Medium Voltage and Systems Business Unit in the Siemens Energy Management Division. "By adding the SF6-free 8DJH 12 model to our portfolio, we are continuing the story of blue GIS medium-voltage switchgear. The switchgear meets the requirements of tomorrow while providing all the familiar 8DJH functionalities, such as the proven operating concept for load-break switchgear, the same compact dimensions, and climate neutrality. Along with sustainability, we are also taking steps toward digitalization. Our goal is to make a future-viable power distribution possible for our customers."
Siemens will present the new switchgear for the first time at Hannover Messe as part of the "Future Distribution Substation".
For further information on Division Energy Management, please see www.siemens.com/energy-management
For further information on the 8DJH 12 switchgear, please see www.siemens.de/8djh12
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.