Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release08 September 2022Smart InfrastructureZug
Siemens equips its Intelligent Valve with glycol capability and change-over function
Thanks to the newly integrated dynamic control change-over function, a heat
exchanger can be dispensed within the assembly of AHUs. Intelligent Valve has
two different parameter sets: one for heating, and one for cooling. This allows
ideal operation in cost-effective and space-saving applications like combined
coils in AHUs or combined distributions. With its new control function for
changeover applications, the Intelligent Valve automatically detects whether it
is in heating or cooling mode and optimizes quantities such as volume flow or
ΔT. This change-over function saves engineering time and investment costs at
the automation level. The new function allows ventilation centers to be
optimized, AHUs to be downsized, and ultimately space to be saved that can be
used for other purposes.
Visit
us at Light + Building 2022 in Frankfurt am Main, October 2 - 6, in hall 11.0,
B56.
For further information on Siemens Smart
Infrastructure, please see
www.siemens.com/smart-infrastructure
www.siemens.com/smart-infrastructure
For further information on Intelligent
Valves, please see
www.siemens.com/intelligentvalve
www.siemens.com/intelligentvalve
For this press release
Follow us on Twitter
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2021, the business had around 70,400 employees worldwide.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2021, which ended on September 30, 2021, the Siemens Group generated revenue of €62.3 billion and net income of €6.7 billion. As of September 30, 2021, the company had around 303,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
In fiscal 2021, which ended on September 30, 2021, the Siemens Group generated revenue of €62.3 billion and net income of €6.7 billion. As of September 30, 2021, the company had around 303,000 employees worldwide. Further information is available on the Internet at www.siemens.com.