Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release27 August 2015MobilityMunich
Siemens automates New York subway line
Siemens is supplying the onboard equipment for a total of 305 trains and installing the wayside signaling technology at 7 of 8 field locations. Through automated signals and sensors throughout the line, the CBTC technology provides continuous updates on system status that results for fewer delays and up-to-date travel information shared with riders via public address systems, electronic screens and mobile applications. The system also reduces the amount of wayside equipment and employs back-up systems, resulting in fewer instances of service disruption and greater reliability.
With a length of around 43 kilometers, the Queens Boulevard Line is the second longest line in the New York subway network. It has 25 stations, from Jamaica Station in the Borough of Queens in the east to Manhattan, the center of the New York business world. Many commuters use the line to travel to work from their homes in the suburbs and, with a daily volume of over 250,000 passengers, it is one of the most heavily used lines in this metropolis.
Every day, over five and a half million passengers ride the over 100-year old New York City subway system. To keep pace with the increasing number of passengers, the system is continuously being modernized. In addition to the new system on the Queens Boluevard line, Siemens successfully installed CBTC technology on MTA's Canarsie "L" line that operates from Chelsea (Manhattan), through Williamsburg to Canarsie (Brooklyn). The automation technology has allowed MTA to handle and sustain increasing ridership on the line over the last 20 years.
Siemens CBTC solution Trainguard MT is the most extensively deployed automatic train control system and is used by more than 20 metro operators around the world including Paris and Beijing. This is Siemens' fifth CBTC project in the U.S.
Links
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 343,000 employees worldwide on a continuing basis. Further information is available on the Internet at www.siemens.com.
Contact
Katharina Ebert
Siemens AG
Otto-Hahn-Ring 6
80333 Munich
Germany
80333 Munich
Germany
+49 (89) 636-636802