Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release30 June 2017Energy ManagementErlangen
Siemens and Vietnamese energy company EVN open a new main control center for 21 provinces

The picture shows the new main control center in Ho Chi Minh City
"EVN's new network control center enables it to respond flexibly and cost-efficiently to the current and future challenges of ensuring reliable network operation. For EVN, that means an improvement in both its operational efficiency and quality of service", said Thomas Zimmermann, CEO of the Business Unit Digital Grid, Siemens Energy Management Division.
"We are very excited with the opening of the main control center SCADA DMS in Ho Chi Minh City. Equipped by Siemens most advanced technology in the power distribution industry the center will help us to remarkably improve the efficiency and reliability of the distribution network in 21 provinces and cities in the southern region of Vietnam. We will be able to create sustainable values not only for the region but also our company through higher productivity and significant cost savings", said Mr. Nguyen Van Hop, President and CEO of Electricity of Vietnam Southern Power Corporation (EVN SPC).
The control center technology is based on the Siemens Spectrum Power system platform for network control centers, which will be used in Vietnam as a SCADA and distribution management system (DMS). However, the control center will not only be used for remote monitoring and control of distribution grids with capacities of 110 kilovolts (kV) and below, but it also can work with the transmission grid (220 kV and above) in order to minimize losses and down times. With the aid of the Siemens grid control technology, the state-run energy company will also prepare 110 kV transformer substations for unmanned operation in the future.
SCADA (Supervisor Control and Data Acquisition) systems are used to operate and observe, control and monitor power grids, while the distribution management system with which they are combined optimizes distribution grid management. The Spectrum Power SCADA/DMS system from Siemens enables grid operators to control the grid management system and the energy flow. The system can be operated locally or remotely thanks to its web-based architecture. In addition, it helps to reduce grid maintenance costs and eliminate faults faster.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Dietrich Biester
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 7-33559