Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release29 May 2018Process Industries and DrivesNuremberg
Rugged Industrial Ethernet switches for the process industry

The picture shows the new versions of the Scalance X-200, Scalance XF-200BA, Scalance XC-200EEC and Scalance XP-200EEC managed product line.
The new versions of the Scalance X-200, Scalance XF-200BA, Scalance XC-200EEC and Scalance XP-200EEC managed product line have all the hardware properties required in the process industry: lacquered PCBs (conformal coating), extended temperature range (-40 to +70 degrees Celsius), installation altitude up to 4000 meters and conformity with Namur NE 21. Special bus adapters, such as the BA 2xRJ45VD HA, allow existing Profibus cable infrastructures to continue to be used, and Profinet devices can be connected to the Profibus network from a distance of up to 1000 meters without additional amplifiers
The Scalance XF204-2BA switch has a flat type of construction and versatile bus adapters for a flexible network structure with copper or fiber-optic cables.
Scalance XF204-2BA DNA Y-switches also have a flat type of construction and are suitable for connecting Profinet S2 devices to a redundant controller (AS) as an R1 system. Bus adapters support a flexible network structure.
The gigabit-capable Scalance XC-200EEC switch is used as a service bridge for protected access from a system bus to a field bus, for the construction of structured networks in the field area with line, ring or star topologies, and for connecting multiple electrical or optical Profinet devices.
The gigabit-capable Scalance XP-200EEC switch is suitable through its high IP65 degree of protection and rugged M12 connector system for cabinet-free use and for supplying PoE-capable terminal devices, such as IP cameras.
For further information, refer to www.siemens.com/switches-for-pa
Find further information about Siemens at the Achema 2018 at www.siemens.com/achema and www.siemens.com/press/achema2018
For this press release

Event: Achema 2018
Press Event
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616