Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release14 February 2019Energy ManagementErlangen
powermanager power monitoring software with direct cloud connection

The picture shows the software powermanager.
In combination with communication-capable protection and measuring devices, such as 3VA molded case circuit breakers and 7KM PAC measuring devices, the powermanager power monitoring software establishes the technical basis for operational energy management according to ISO 50001 and ISO 50003. The scalable and intuitive software can be easily deployed with the available hardware and the existing IT infrastructure. Among other features, the power averages of the characteristics monitored are visualized as graphs showing changes over time on the user's PC, and load peaks are quickly identified. Through the direct comparison of various processes, loads or system components, inefficiencies can be uncovered. Loads can be allocated exactly and on a cross-location basis to individual cost centers – this enables precise benchmarking, along with optimization of utility contracts. Thanks to continuous monitoring of power distribution, even critical plant states are identified early, and downtimes are prevented. Users can benefit from a considerably higher plant availability and energy efficiency, along with lower costs.
More information on electrical power distribution in the digital age is available at www.siemens.com/lowvoltage/digitalization and www.siemens.com/powermonitoring
More information on Siemens at the Hannover Messe 2019 is available at www.siemens.com/hannovermesse
More information on Siemens at the Hannover Messe 2019 is available at www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Heidi Fleissner
Siemens AG
Siemensstr. 10
93055 Regensburg
Germany
93055 Regensburg
Germany
+49 (941) 790-2212