Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release15 November 2018Energy ManagementErlangen
PG&E to use SF6-free high-voltage products from Siemens

PG&E to use SF6-free high-voltage products from Siemens

PG&E to use SF6-free high-voltage products from Siemens
"In recent years, Siemens has been hard at work developing a new generation of high-voltage products that offer outstanding performance and sustainability. Our goal is to offer SF6-free high-voltage products preferably on all voltage levels in power transmission. They can already be used in many sectors," explains Ralf Christian, CEO of the Siemens Energy Management Division.
"We're happy to be joining PG&E in taking the next steps toward sustainable power transmission with no greenhouse gas emissions and to implement the easiest possible operating and recycling processes. This is one way that we're doing our part to achieve the global climate protection targets," says Beatrix Natter, CEO of the Transmission Products Business Unit within Siemens Energy Management. The 3AV1 DT dead-tank circuit breakers offer a rated voltage of 115 kV, a rated short-circuit breaking current of up to 40 kiloamperes (kA), and a rated current of up to 3,000 amperes (A). The 8VN1 GIS feature a rated voltage of 115 kV, a rated short-circuit breaking current of 50 kA, and a rated current of 3,000 A.
SF6-free circuit-breakers and GIS are a further development of insulation using SF6, which has been proven in practice for years. A modern vacuum interrupter unit handles the switching and arc-extinguishing functions. Industrially prepared and purified air in a mixing ratio of 80 percent nitrogen to 20 percent oxygen (known as "clean air") provides the insulation for the current-carrying conductors inside the housing. Siemens has developed its existing technology to meet climate neutrality requirements by combining vacuum interruption systems for switching and for arc extinguishing with "clean air" as the high-voltage insulating medium.
The first milestones in SF6-free switching technology from Siemens were the successful deployment of vacuum interrupters in outdoor circuit breakers, which have been in use since 2010. SF6-free GIS for 72.5 kV have been used in wind turbines and the first SF6-free outdoor circuit breaker in the German 110-kV high-voltage grid since 2018. The benefits of this technology over conventional SF6-insulated switchgear are significant: high switching power with the same footprint for outdoor and dead-tank circuit breakers. The products can be operated at lower temperatures without their own heating systems, and the switching unit requires no maintenance. They don't require F-gas reporting during operation and are much easier to recycle. "Clean air" can be released into the atmosphere with no harmful effects. The circuit breaker has a lifecycle of 40 years, which is the same as the variants with SF6. The products therefore meet global manufacturer and grid operator targets with respect to climate-neutral operation, decarbonization, and sustainability.
Pacific Gas and Electric Company, a subsidiary of PG&E Corporation (NYSE: PCG), is one of the largest combined natural gas and electric energy companies in the United States. Based in San Francisco, with more than 20,000 employees, the company delivers some of the nation's cleanest energy to nearly 16 million people in Northern and Central California.
For further information on the Siemens blue portfolio, please see siemens.com/eco-transparency
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2018110065EMEN