Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release28 March 2019Digital Factory Nuremberg
New Simogear Reluctance Geared Motor – compact, rugged, and energy efficient
The picture shows a synchronous-reluctance drive system.
Maintenance and repair work is easy thanks to the modular design of the system. The motor is very energy efficient, hardly heats up at all, and therefore runs safely due to this excellent thermal behavior and the overload capacity, even at high speeds, mentioned previously. Optimum functionality of the drive system is provided by the interaction of the reluctance motor, gear unit, and converter which are precisely matched to each other. This results in economical operation and efficient performance of the entire drive system.
For further information regarding the Simogear, please see www.siemens.com/simogear as well as at the Siemens booth D35 in hall 9 of the Hannover Messe.
More information on Siemens at the Hannover Messe 2019 is available at www.siemens.com/press/hm19 and www.siemens.com/hannovermesse
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Katharina Lamsa
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (9131) 17-35398