Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

New measuring devices simplify power monitoring in buildings

The picture shows the multichannel current measuring system SEM3.

The multichannel current measuring system SEM3 is used in the main power distribution and consists of current transformers, measurement modules and a central controller. The scalable complete system can detect up to 45 measurement points in a building. The power data such as voltage, currents and power can be visualized in a single web interface or in the powermanager power monitoring software. This makes it possible to directly compare individual loads and to identify current peaks. Systematic power monitoring promotes greater energy efficiency in buildings and creates the technical basis for certification according to ISO 50001. The multichannel current measuring system SEM3 fulfills all requirements of the standard. The system makes energy consumption transparent, energy hogs are identified, and increased electricity costs are avoided. The internal cache (two gigabytes) allows for the storage of long-term data. Retrofit installation in existing power distributions is possible at any time.
The new compact 7KT PAC1600 measuring devices are installed using a space-saving design in power and installation distribution boards. They detect base electrical quantities and show the values directly on the display of the relevant measuring device. Special device versions are tested according to the European Measuring Instruments Directive (MID). MID certification enables the costs for the measured energy consumption to be billed to third parties. The user-friendly devices with a display are available in single-phase and three-phase versions, each with special MID certified versions. Via an integrated communication interface, the detected energy data can be transmitted via Modbus RTU and M-Bus to higher-level energy management or billing systems – and this does not require any additional communication modules.

For further information on Division Energy Management, please see www.siemens.com/energy-management
For further information on power monitoring, please see www.siemens.com/powermonitoring
More information about the Light+Building can be found at www.siemens.com/press/lightbuilding-2018
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2018030205EMEN

Contact

Heidi Fleissner

Siemens AG

Siemensstr. 10
93055 Regensburg
Germany

+49 (941) 790-2212