Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release18 February 2019Digital Factory Nuremberg
New generation of high-end industrial PCs – high performance and flexibility in the industrial environment

The picture shows the four new Simatic units.
All devices have up to 64 GB DDR4 RAM, an M.2 NVMe SSD storage medium, 3x Gigabit Ethernet for high productivity even in demanding tasks, plus USB 3.1 Gen 2 (SuperSpeedPlus) in the USB Type A and Type C versions for fast service and maintenance jobs. The new IPCs are designed for 24/7 continuous operation and are also suitable for environments subject to high levels of vibration, shock and EMC emissions, as well as ambient temperatures up to 50 degrees Celsius.
The integrated Intel AMT (Active Management Technology) enables convenient remote management for secure remote diagnostics and maintenance. All devices also feature fast system diagnostics with status LEDs and pre-installed DiagBase diagnostics software. The new enclosure concept was especially constructed for even faster device modification. The Simatic IPCs come with the option of a pre-installed Windows 10 Enterprise 2016 LTSB or Windows Server 2016 operating system. E generation devices have up to 100 percent more performance than the predecessor models of the D generation, whatever the configuration.
Users can choose Intel Core i7, Core i3 or Celeron for their compact Simatic IPC627E box PC. The Simatic IPC677E panel PC version with full HD display in 19", 22" and 24" is available for central operator control and monitoring.
The 19" rugged Simatic IPC 647E industrial PC is available with Intel Xeon, Core i7, Core i5 or Core i3 and, thanks to its small height (2U) and installation depth, is ideal for the space-saving implementation of high-speed computing and visualization tasks, such as in image and data processing or industrial server applications.
The Simatic IPC847E can be expanded with up to 11 slots and, due to its high system availability, computing power and PCI Express technology, enables the user to perform high-end image processing – for example in quality inspection, or manufacturing-level data acquisition and processing.
Moreover, the IPC847E keeps operations running in harsh industrial environments, even withstanding large amounts of dirt, extreme temperatures and high shock loads.
Moreover, the IPC847E keeps operations running in harsh industrial environments, even withstanding large amounts of dirt, extreme temperatures and high shock loads.
For further information, refer to www.siemens.com/ipc
For further information on Siemens at the Hannover Messe 2019, please see www.siemens.com/press/hm19 and www.siemens.com/hannovermesse
For further information on Siemens at the Hannover Messe 2019, please see www.siemens.com/press/hm19 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Andreas Friedrich
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (1522) 2103967