Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release23 February 2017Building TechnologiesZug
Intuitive operation and increased flexibility for Desigo building management system

The picture shows numerous new components and functions of the modular Desigo CC building management platform.
The user-friendly Desigo Control Point solution is one of the main innovations in the new version of Desigo. It offers building management functionality via web access and state-of-the-art touch panels. A graphical user interface allows users to operate HVAC, lighting and shading disciplines. The solution also allows energy dashboards to be created for managing and analyzing the energy footprint of the monitored systems.
The new PX Compact Controller with island bus complements the Desigo family. It can be flexibly expanded with TX I/O modules to cover a greater number of data points. In combination with TXI2.OPEN, the compact controller also offers various integration options.
One key component of the room automation portfolio of the new Desigo version is a solution for room pressurization and fume hood control specially developed for use in laboratories and clean rooms. This solution communicates via BACnet/IP and ensures reliable, precise and fast measurement, control and monitoring of air volumes and room pressures. The room automation portfolio now also includes a new KNX PL-Link rotary actuator which is designed for use with 6-way ball valves, as well as a new KNX-PL link light dimmer and new cost optimized room operator units. The functionality of the Desigo Room Automation applications is also extended to include heat pump application types further complimenting the existing application suite.
Finally, Desigo offers new migration paths that ease the switch from Siemens existing management stations to the comprehensive Desigo CC building management platform.
For further information on Desigo, please see www.siemens.com/bt/de/desigo
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet atwww.siemens.com.