Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

High-performance Simotics DP roller table motor for extreme conditions

The picture shows the Simotics DP roller table motor from Siemens.

The standard versions of the Simotics DP roller table motors are classified in compliance with protection rating IP66. They can optionally be fitted with an additional "special sealing system – corrosion protection" to withstand exceptionally tough environmental conditions. Their vibration and shock resistance is tested and confirmed in exhaustive test lab trials.
The series is based on the new motor platform 1LE1 and is designed to supplement the existing Simotics DP steel mill motors in sizes 112M-200L, making this a one-stop solution for all kinds of transport applications in the metalworking industry. This not only reduces any associated risks but also makes for more efficient project engineering.
Simotics DP roller table motors are ideally suited for operation in conjunction with the SINAMICS S120 converter. Operation of this combined system has been exhaustively laboratory tested.

For further information on topic Simotics DP, please see www.siemens.com/simotics-dp
For further information on Siemens at the Hannover Messe 2017, please see www.siemens.com/press/hm17 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2017040255PDEN

Contact

Stefan Rauscher

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7952